My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
DHL account
We have DHL account already. Please give us an option to use our own DHL account.
3 votes -
make a tool to update the rephone firmware from Linux or at least Windows 10.
I spent money and nothing works without a firmware update, I have Ubuntu and Windows 10 machines, advertised as open source, then tell me how to use any tool to update the firmware, it cannot be that complex, set in to firmware loading mode, transfer. bin file, disable firmware loading mode. or give me a couple of hundred dollars of credit for the money you took from me and lied to get, you have lots of great products and rephone should be one of the best but it isn't versatile enough to develop on. mac and Linux support will make…
3 votes -
Hi people. Re Bus Pirate V4. Screw hole size change to suit case.
Hi people. Re Bus Pirate V4. The acrylic case kit has 3 mm screws, but the screw holes on PCB are only 2.8 mm after plating, and plating is used as part of ground connection, so drilling out is undesirable. Suggest you use 3.3 mm holes pre-plate on any rerun of boards.
3 votes -
PCBA with < 50 pieces/board cost much more than PCBA with > 50 pieces???? Why
I do calculation from your PCBA specification and I see board with < 50 pieces cost $0.10 per pin and board with > 50 pieces cost $0.01 per pin.
This pricing policy of yours means that a simple board cost more than a complex board.
This is a silly policy. We are looking for a manufacturer to produce thousands of boards for us, so I think we will use a different company because your cost is bad.3 votes -
I2C_LCD Grove I2C Address
I like that little screen, but its I2C address of 0x51 is REALLY annoying. Traditionally, 0x50 to 0x57 is reserved for external EEPROM chips. By setting the I2C address of this LCD to 51, I lose one slot for my EEPROM chips, and I have to rewrite code. Could I suggest you produce the next version with an I2C address that doesn't conflict with existing standards?
3 votes -
to make a good search field. When I describe a product like 'solar shield' I get all kind of products, even not related to solar!
to make a good search field. When I search a product like 'solar shield' I get all kind of products, even not related to solar or shield!
It was good before, but now it's completely messed up!!!!
3 votes -
Don't use DHL for Italy
Crazy extra cost with DHL. I ordered 110$ and I payed 50$ of extra taxes. I think that I will never order material from seed studio site!
3 votes -
Update the Relay Shield to Version 4.0 with....
The arduino relay shield could be even better with:
1) If the status LED's were in order for 1, 2, 3 and 4.
2) If the shield used smaller reed relays and supported 6 or 8 relays.
3) If each terminal block had FOUR terminals one unused. Why? Because there's always a ground return or something else to hook up.
4) If there were a solder block so the pins activating the relay could be cut and swapped to other I/O pins.
5) If the silk screen documented what I/O pins went to each relay by default.and
6) If…
3 votes -
Your mobile site stinks
Include the option to choose desktop site view on all devices.
3 votes -
Exclude discontinued items from listings.
It's getting where there are more discontinued items than new ones. It would be nice if the discontinued items were only visible if you visited the item directly. (Preventing broken links). Otherwise exclude them from the default view.
3 votes -
UPS board for generic SBC
There are few boards with native lithium battery support but it would be nice to add UPS like function to any 5V powered board, be it ARM or Atmel. AXP209 is integrated on some boards and I believe it would be very interesting to have it on a breakout board similar with a solar charge controller. The simplest configuration would have only 6 pins (5V--In&GND / Batt+&Batt- / 5V-Out&GND). Some extra feature would make it even better: an EN pin that would cut-off both battery and Vin input. An AO pin to measure the battery voltage, a DO to send…
3 votes -
To make lead free PCB - it will bring to you new customers
To produce lead free PCB is very importent in europe!
Companys will chose factorys with that ability3 votes -
3 votes
-
Make logins last longer
While assembling a recent order over several days, I was very frustrated by how often I had to log in. I can understand asking for my password before placing an order or viewing account details, but I just wanted to see the items in my cart. I don't think meaningful security is gained by not letting me stay logged in.
3 votes -
non-OPL PCBA Ordering Instructions
Add instructions about how to order PCBA when not all parts are in the OPL
3 votes -
Cart sharing capability. I would like to send the cart to my supervisor by email.
Cart sharing capability. I would like to send the cart to my supervisor by email.
3 votes -
Shipping cost to Russia & ex-USSR countries. Make it fast, cheap, predictable.
You can use SPSR/CDEK/Pony Express for Russia & ex-USSR countries. Only 5-15$ per small packet . Fast & predictable.
3 votes -
3 votes
-
DipTrace gerber export tutorial incorrect (twice)
In your tutorial regarding how to export gerber files from DipTrace, you show the resulting output files as all having .gbr extension, yet your standard is for the extension to indicate the type of file and for each file name (sans extension) to be the same. That is misleading.
Also, you show a set of Gerber file types highlighted in the Layers box. This will NOT limit the output to only those file types. When you hit the "Export All" button it will, literally, Export ALL of the file types, not just the ones that were highlighted.
There is a…
3 votes -
Raspberry Pi support for Grove-TF Mini LiDAR
Raspberry Pi support for Grove-TF Mini LiDAR
3 votes
- Don't see your idea?