My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
Contact Seeed
Why don't you guys answer your emails? All I get are canned responses.
4 votes -
Beagle Bone Green Wireless Without the Dual Stacked USB Connectors
The Beagle Bone Green Wireless is a great idea for several reasons. One thing I was looking for was to get ride of the bulky Ethernet connector. This is an embedded board that is already big, because of the .1" headers, it is humongous in height because of the Ethernet connector.
And so when the wireless version came out I was ex-tactic for a second until I realised you added 2 dual stacked USB connectors?!?!
Please leave the choice to the user to decide whether or not they need that much real estate wasted.People who have enough space for…
4 votes -
Add a way to confirm receiving of parcel with order
I received my orders some days ago but its status still "Traceable"
4 votes -
finding cheaper shipping options
Cheaper shipping
5 votes -
Persistence of Vision Board.
Peristence of Vision Board.
Hi I'd like to share a project of Persitence of Vision: Arduino code generator for images and text. It is DIY cheap and easy, and all resources are free.(load any image and it gearates the code)
http://persistenceofvisionproject.com/
Thanks.
4 votes -
Delivery Estimates
What is the estimated days to delivery?
4 votes -
Virtual DJ 8
Virtual DJ 8 Free Download With Latest Version. Virtual DJ 8 is most used Dj software in the world.
https://softmega.org/virtual-dj-8/4 votes -
Budget Shipping option
I ordered a few boards a month or so ago and the only shipping options were DHL and I forget what other service but it was even more expensive. Might I suggest a budget shipping option for those customers who are less concerned with longer lead times such as say post. The two board orders I placed cost $13.50 CAD and shipping was $35. Then on top of that the boarder stung me with $26 in tax a duty which I do not understand how they can charge more than the product is worth, a problem I have only ever…
4 votes -
sort OPL items
OPL items should be sorted by some meaningful criteria; it is hard to choose a specific item among 15000 different ones. If it is not possible, it should be possible to download all the data base, let's say in Excell format, an do ourselves the sorting by different criteria (case size, manufacturer, name, etc.)
4 votes -
Wire harnesses assembly
Please add a assembly service for custom wire harnesses
4 votes -
3 votes
-
HS code
you should post an option of "the number of harmonized system code or the number of tarif code" for international purchases.
3 votes -
Seeeduino 1284P
I would like a Seeeduino 1284P. I really like Seeed's configuration of
the mega better than arduino's, however I feel that the 1284p has
the right amount of I/O and storage with more RAM than the 2560.3 votes -
payment method
Better, more reliable payment method.
3 votes -
Pass the shipping consignment number to the tracking site.
Pass the shipping consignment number to the tracking site.
The order tracking popup is a terrible way to incorporate order tracking: use a proper page or a panel on the base page. I can't select text from the layered panel on my tablet browser.
The track order link doesn't seem to pass the consignment number, which would make sense.
3 votes -
BT blink sound for bikes
Needed a simple beep or sound generator and a bluetooth sending device with a common BT protocol in a water resistant housing on base of 12 V and a trigger input (or two).
The trigger could be connected with the blinking relais, controling light or the two blinking lights.-> EASY, SIMPLE but VERY valuable for bikers, because they could hear the blinking INSIDE the helmet, while OUTSIDE beepers are forbidden for being too loud for the surrounding to be heard inside the helmet while cruising fast speed.
I think this gadget should be sold very often, because its very…3 votes -
We need a MagnetoPot Potentiometer in Grove ...
http://www.spectrasymbol.com/potentiometer/magnetopots
Build us a MagnetoPot Potentiometer leaf to plug into Grove. This will allow the monitoring and response to motion using a solid state contactless sensor. These particular Pots monitor over a longer range of motion so will be highly flexible and useful in there applications for many projects and Grove user applications.3 votes -
Bought a Grove starter kit for Arduino : poor support
I was used to working with straight forward Arduino, just fine, Thought the plug-and-play of grove was a good idea.
But the information to get it working is poor. The links on the paper do not exist anymore. No clear starting instructions what to install where exactly to get it going. Much information seems to be implicit.
Information is just not complete and/or easy to understand. Pieces are missing. You-tube?3 votes -
Your Verification button says its case sensitive but codes only show upper case. In short it dont work!
Fix your Verification box so that it shows both upper and lower case letters properly. I do not have time to be dicking around trying to figgure this out.
3 votes -
DHL account
We have DHL account already. Please give us an option to use our own DHL account.
3 votes
- Don't see your idea?