I suggest Seeed...

Update the Relay Shield to Version 4.0 with....

The arduino relay shield could be even better with:

1) If the status LED's were in order for 1, 2, 3 and 4.
2) If the shield used smaller reed relays and supported 6 or 8 relays.
3) If each terminal block had FOUR terminals one unused. Why? Because there's always a ground return or something else to hook up.
4) If there were a solder block so the pins activating the relay could be cut and swapped to other I/O pins.
5) If the silk screen documented what I/O pins went to each relay by default.

and

6) If the LED's were side view type, so they could seen even if another shield is on top. Maybe even put them next to the connector they control?

3 votes
Vote
Sign in
Check!
(thinking…)
Reset
or sign in with
  • facebook
  • google
    Password icon
    Signed in as (Sign out)
    You have left! (?) (thinking…)
    Bryce Nesbitt shared this idea  ·   ·  Admin →

    1 comment

    Sign in
    Check!
    (thinking…)
    Reset
    or sign in with
    • facebook
    • google
      Password icon
      Signed in as (Sign out)
      Submitting...
      • Bryce Nesbitt commented  · 

        And... add a couple of large holes for tie wraps, on the edge of the boards. So wires coming into the relays can be properly dressed and secured.

      Feedback and Knowledge Base