My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
Put the Eagle DRU files back onthe specifications page.
Seeed used to provide Eagle design rules files (DRU) for 2 and 4-layer boards. They seem to have been removed...
71 votes -
To make the gerber viewer available for past orders
When viewing the order history it is possible to reorder past orders. It would help a lot if it was possible to view PCB's in these orders - it would at least increase the likely hood that one actually does reorder something.
58 votes -
translation service
Shakespeare Language Service is very professional. Projects were delivered on time and accurately translated, unlike another agency I used before. Fast turnaround. Would highly recommend their service to others! Their Website: https://www.shakespeare-translation.com/
54 votes -
Bitcoin payments
bitcoin is easier and cheaper than shitty credit cards. Adafruit.com and many chinese PCB manufactureres already accept it.
43 votes -
Fusion PCB pricing
PCB should be priced by the total sq cm used & not by fixed length & width measurements. This would stop crazy price jumps. Build a board that is 5.54cm & you have to move up to 10cm size board pricing. This crazy & shouldn't be happening. Please price your boards fairer for the total area of the boards used & not for the area not used.
29 votes -
stop overcharging for shipping Fusion PCBs
Please charge customers for the correct shipping weight instead of the maximum for PCBs of any given size. Most companies do this.
For an example, Arduino (shield)-sized boards are only one third the size of the 10cm x 10cm board category that must be used to buy them, but they are only ONE THIRD of the size and weight. We have to pay (express) shipping for TRIPLE the weight of the actual order and this can be substantially more expensive.
Please use the actual board size to compute the proper weight. Many other lower-cost PCB prototyping services do this, and…
23 votes -
Fusion PCB Specification -- Provide separation dimensions between layers.
For computing strip-line impedance it is important to know the distance between conducting layers and the dielectric constant of the insulator material. If averages are provided please also provide variance
21 votes -
21 votes
-
robust forgot password system
Verify that the "forgot password" system works.
19 votes -
Add an easily downloadable Eagle DRC file to the website
Add the EAGLE DRC for download
19 votes -
Add Singapore Post to South America Shipping Plase
Add Singapore Post to South America Shipping Plase
17 votes -
International shipping cheaper
Hello friends am a teacher and want to buy "LinkIt 7688 Smart Duo" to teach my students, the problem is that sending to my country (Chile) is very expensive.
So I wanted to know if you have some method of cheaper international shipping.
Because in my country teachers earn little money
Other stores sent by regular mail and is slower but cheaper
Thank you very much.14 votesDear friends,
Pls kindly choose the registered air parcel as the delivery option. It is the regular mail shipping, delivery time is 15-30 business days.
Registered air parcel shipping is available in South America.
Thanks. -
Gift Cards
It would be nice to be able to purchase gift cards in varying amounts from the Seeed Studio store to give out as gifts.
13 votes -
Order Number: 154481
The problem is still not resolved. Waiting for your attention.
Your customer service is progressing very slowly. Problem solving long.
13 votes -
Arduino Dial Up Modem shield
Dial Up modem's days are long gone but Land line still exists either in the form of home pbx or PSTN, An Arduino based Dial Up modem shield can be used for a lot of fun projects.
Modem chips are already available with AT Command support
Currently there is no shield to interface arduino with phone line
This shield can also become a base for Arduino corded telephony with additional sheilds for setting up arduino based Home PABX e.g 4 port intercom shield or Voip shield12 votesThat’s a gooood idea, we’re going to start it from forum.
-
Please include a .pdf version of the Eagle Schematic files
Please include a .pdf version of the Eagle Schematic files for people who don't own Eagle Licences, it would be very helpful. Thanks!
In particular I'm looking for the schematic for seeed arch gprs v2
12 votes -
replace generic icon with pcb render
on the account order history page pcb orders should have a rendering of the board instead of that generic icon
14 votes -
Altium library
id like to see an altium library. could even host it somewhere and the community could keep it updated / reviewed. i wouldn't mind helping create some parts.
11 votes -
More information needed on out-of-stock items
More details need to be given for out-of-stock items. For example, is it being replaced? Will it be available again? When is the ETA?
For example, I have a client who needs 12 new BeagleBone Greens. They've been marked as out-of-stock for a long time now. Is this permanent? Or temporary? What do I tell my client?
11 votes -
to have a filter on 'discontinued' products and not show them in the search bar by default
to have a filter on 'discontinued' products and not show them in the search bar by default
11 votes
- Don't see your idea?