BT blink sound for bikes
Needed a simple beep or sound generator and a bluetooth sending device with a common BT protocol in a water resistant housing on base of 12 V and a trigger input (or two).
The trigger could be connected with the blinking relais, controling light or the two blinking lights.
-> EASY, SIMPLE but VERY valuable for bikers, because they could hear the blinking INSIDE the helmet, while OUTSIDE beepers are forbidden for being too loud for the surrounding to be heard inside the helmet while cruising fast speed.
I think this gadget should be sold very often, because its very cheap to built and easy to implement into the bike by nearly everybody. On the other hand practically very interessant for every biker.
Yours
Peter

-
用户
Jeffery Ollsan 评论
Dirt bikers normally go to great lengths to find the ideal dirt bike tires that will give them the best traction and prevent them from slipping.
Tires are available in a variety of designs and patterns. For the top MX tires, you should get the Motocross tire. However, if you want to find the best rear dirt bike tire, make sure to look at the product's quality and feedback.
Read full guide here https://dirtbikeadvisor.com/best-dirt-bike-tires/ -
用户
Leffler Hirthe 评论
Maybe sounds is the problem. Try for other sound at this site: https://dzwoneknatelefon.com/
-
用户
Hegmann Kris 评论
You need to install additional sound effects for your device. Check this for sound ringtones: https://sonnerieportable.com/
-
用户
Karlis Robert 评论
Where can i find those sounds?
Find out more 2020 favorite songs and ringtones at: https://sonneriepro.com/ , https://sonneriepro.com/iphone/ -
用户
TerryGreer 评论
I have no idea about BT blink sounds for bikes. You can check https://10ebikes.com/recommended-electric-bike-accessories/ this list, there are accessories that can be added on bikes.
-
用户
giniva 评论
Can I get these at walmart stores?
Thanks
https://walmartone.live