make a tool to update the rephone firmware from Linux or at least Windows 10.
I spent money and nothing works without a firmware update, I have Ubuntu and Windows 10 machines, advertised as open source, then tell me how to use any tool to update the firmware, it cannot be that complex, set in to firmware loading mode, transfer. bin file, disable firmware loading mode. or give me a couple of hundred dollars of credit for the money you took from me and lied to get, you have lots of great products and rephone should be one of the best but it isn't versatile enough to develop on. mac and Linux support will make you make more sales and money, why not fix this problem, it has been a year since kicksstarter
![](http://www.gravatar.com/avatar/3aa8d92d13050dc057ba72005bcff0dd?size=40&default=https%3A%2F%2Fassets.uvcdn.com%2Fpkg%2Fadmin%2Ficons%2Fuser_70-6bcf9e08938533adb9bac95c3e487cb2a6d4a32f890ca6fdc82e3072e0ea0368.png)
-
Hi Jamie Roberts,
I am very sorry to tell you RePhone is not support for Linux. But it is could support for Windows 10, I can update firmware on Win10 machine. You can make a try and the way is same to Windows 7.
Thanks.
Wayne Weng/SE