robinmalhotra
My feedback
-
58 votesUnder Consideration · 6 comments · My Seeed Idea » I suggest · Flag idea as inappropriate… · Admin →
An error occurred while saving the comment -
123 votes
An error occurred while saving the comment robinmalhotra commented
I bought a defective Blackwidow Ultimate some time ago, thinking that I would replace some switches and it would be fine. However, it turned out that the switches were fine, and there was a deeper problem.
I searched the internet for my problem, and found some posts with similar cases, but no good solutions (just the usual baths in water and soap). A month or two ago, I started playing with it, and I was able to fix it.
Since I wasn't able to find anything on the internet, I wanted to write my experience with the problem and how I fixed it, hoping that it will help someone with the same problem. I know it is quite long, but I wanted to leave everything clear, and I don't know how to write short texts. I hope it's readable. :P
https://appsync.biz/speed-test/ https://appsync.biz/scrabble-word-finder/ https://appsync.biz/solitaire/ -
5 votes
An error occurred while saving the comment robinmalhotra commented
Was wondering if anybody wanted to share their experiences with regards to purchasing or otherwise engaging with businesses on Flippa...?
https://appsync.biz/speed-test/ https://appsync.biz/scrabble-word-finder/ https://appsync.biz/solitaire/ -
1 vote
An error occurred while saving the comment robinmalhotra commented
Context: I tutor basic coding to people privately and semi-privately. Lately I've had more of the semi-privately (2 or 3 or 4 students at a time) classes, so I set up a projector in my officetel so that the students could all easily see my screen without craning their necks. Instead of hooking up a laptop or desktop to the projector, I found it more convenient to hook up an old Raspberry Pi with a wireless keyboard and mouse.
Specifically it's the original Raspberry Pi 1 B. For those who don't remember the old Raspberry Pi 1 Bs, the specs are:
Single-core 700MHz ARM (roughly comparable to a 300MHz Pentium II)
512MB RAM, shared with video (about 430MB available)
HDMI out
USB 2.0 and an SD reader
https://appsync.biz/abcya/ https://appsync.biz/adam4adam/ https://appsync.biz/pof/ -
15 votes
Dear friends,
Pls kindly choose the registered air parcel as the delivery option. It is the regular mail shipping, delivery time is 15-30 business days.
Registered air parcel shipping is available in South America.
Thanks.An error occurred while saving the comment robinmalhotra commented
I’ve been selling for a few months part time and I always shipped domestic. I was wonder with those who had a lot of experience selling internationally found it worth it.
Are there problems with items arriving to the buyer?
Are returns a hassle?
Does eBay handle the shipping cost or I would have to ship it to the buyer?
Do I have to choose the shipping method or does eBay handle it for me? What type of service do I select?
I sell mostly clothes so I don’t have to worry about fragile things. I’m curious to see if I open up international shipping if it will broaden the clientele
Thank you all in advance
https://appsync.biz/speed-test/ https://appsync.biz/scrabble-word-finder/ https://appsync.biz/solitaire/ -
7 votesUnder Consideration · 3 comments · My Seeed Idea » I suggest · Flag idea as inappropriate… · Admin →
An error occurred while saving the comment robinmalhotra commented
I've had my work laptop for almost three years now. I occasionally connect to our work server through a VPN connection.
How do I make sure that all my personal files and links and etc are really deleted before I turn it back in?
I was not as good as I should have been about keeping personal stuff off of it, but when I traveled for work I didn't want to drag my personal laptop along.
The work files need to be left in the machine. I can't reformat the hard drive or anything like that.
https://appsync.biz/abcya/ https://appsync.biz/adam4adam/ https://appsync.biz/pof/ -
110 votes
An error occurred while saving the comment robinmalhotra commented
Please utilize this sticky thread for all general Bitcoin discussions! If you see posts on the front page or new which are better suited for this daily discussion thread, please help out by directing the OP to this thread instead. Thank you!
If you don't get an answer to your question, you can try phrasing it differently or commenting again tomorrow.
https://appsync.biz/speed-test/ https://appsync.biz/scrabble-word-finder/ https://appsync.biz/solitaire/
-
122 votes
An error occurred while saving the comment robinmalhotra commented
In the options window for the copper fills, there are options to set the type of pad connection. The default will connect the pads by only a few small traces, and the type 'solid' will create a connection that encompasses the entire pad.
Is there any downside to the 'solid' setting?
Sorry if it is not explained well, my KiCad GUI language is not english and even if it were, it's still hard to explain...
https://appsync.biz/abcya/ https://appsync.biz/adam4adam/ https://appsync.biz/pof/
-
5 votes
An error occurred while saving the comment robinmalhotra commented
I usually use an American fab house, but once I needed a bunch of cheap boards for a learn-to-solder class I was teaching. I ordered a batch through Seeed and one or two boards had this unintentional short between a trace and a ground plane. I can't remember exactly what the clearance was supposed to be, but it was well above spec. Pretty sloppy smudge of copper visible below the soldermask. They sent more boards than I ordered, so I can't really complain about getting ripped off, https://appsync.biz/abcya/ but I wasn't expecting this kind of an error on their part. https://appsync.biz/adam4adam/ We had to throw out the kid's board and start over https://appsync.biz/pof/
I've tried several gerber viewers and each has features I like but all are quirky. Lately I've been using GerberLogix (primarily) and ViewPlot (for measuring features). Any other suggestions? Bonus points for "free for commercial use."
https://appsync.biz/speed-test/ https://appsync.biz/scrabble-word-finder/ https://appsync.biz/solitaire/