My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
The 'Contact Support' link to the right doesn't work.
I need to change my shipping address and can't contact customer support because the link doesn't work
2 votes -
Order list page should be re-organized
if you have more than 3 orders it's really hard to quickly find out which one you are looking for, probably a grid view would be more convenient.
1 vote -
Oscilloscope jack connection for probes
I have a DSO Nano Oscilloscope v2, and I would like to connect a normal digital probe to this, but it has 3.5mm jack input. Are there any probe with this specs?
I have the original probes with hook and pins, but I would like to know if is there possible.
1 vote -
my suggestion is for us to parter to create an electronic device to sign in and sign out with biometric
in my country nigeria,most workers get to their placer of work and go through a manual process of signing in,the time they resumed work,my idea is to see how this process can be atomated with a simple electronic device that would have a biometric system in it.where you use your thumb print to sign in.please get back to me so that i can explain better.there is a large market in nigeria for this busines.
0 votes -
More dimensions on the list.
PCB dimension 25x35cm should be available for standart Fusion service. Pcb area is smaller than for 30x30.
6 votes -
LoNet - GSM/GPRS/GPS Breakout
More documentation
9 votes -
make possible to add to wishilst something out of stock
Sometimes i can see something i like to buy. But don't want it now. It is for whishlist is right?
So why I cannot add there items which are temporarly out of stock?10 votes -
Web site fix/improvements
The new user registration page is clearing the Address's State if there is an error. In my case it was the nickname. Then you get an error for that. It also forgets that you entered a captcha. You should only have to do that successfully once as you have proved you are human. There is also no indication that a Nickname needs to be unique. I would rename that Username, which is thus implied. It is also useful to use AJAX to immediately let the user know that a Username is taken, rather than waiting them to press Submit and…
1 vote -
DipTrace support for Open Parts Library
Support DipTrace
6 votesWe will ask Diptrace to import OPL.
Thank you for your feedback. -
433Mhz module
Add 433/868Mhz module to communicate with wireless sensors which work on this frequences.
9 votes -
stop selling old stuff that no longer works....
stuff that works....
0 votesCould you show us what is “old stuff” ?
-
Arduino Dial Up Modem shield
Dial Up modem's days are long gone but Land line still exists either in the form of home pbx or PSTN, An Arduino based Dial Up modem shield can be used for a lot of fun projects.
Modem chips are already available with AT Command support
Currently there is no shield to interface arduino with phone line
This shield can also become a base for Arduino corded telephony with additional sheilds for setting up arduino based Home PABX e.g 4 port intercom shield or Voip shield12 votesThat’s a gooood idea, we’re going to start it from forum.
-
Offer an Intel Edison Arduino IoT Starter kit bundle with everything on one SKU
A complete Edison+Arduino+Starter Kit in one bundled SKU.
0 votesWe have kit for Edison(http://www.seeedstudio.com/depot/Grove-starter-kit-plus-Intel-IoT-Edition-for-Intel-Galileo-Gen-2-and-Edison-p-1978.html?cPath=84_13), maybe other requirements?
-
Create waterproof Grove connectors
If Grove (4 pin) connectors could be waterproof, that would make it easier to use outdoors/in harsh environments.
Wouldn't have to be IP67 or IP68 compliant, just something a bit more robust that what exists.
You'd need bulkhead connectors as well, so you could put a controller/batteries in a waterproof box, and the sensors someplace else.
4 votesHi Andrew:
Thanks for your advice, we believe that waterproof function is important in harsh environments for groves. But since the sensor itself needs to be waterproof, we believe that an enclosure for the whole grove module may be better.
Please let us know your opinion. -
Sign In button jumps left when Facebook button arrives!
In my case [FireFox 33.1.1 on Win 7 64bit] the "Sign In" button jumps left when the slothful Facebook button finally appears. The timing places the Facebook button under my mouse pointer at exactly the same time as perform a mouse click -- hugely frustrating!
I suggest you move the Facebook button to a position under or above the Sign In button.
4 votes -
Seeed ruler
I want to make a geek ruler.This ruler should include common package, trace width, button battery, led. buzzer. Anyone who want to test components whether breakover, he just need to put it on the pad and judge the sound. Also he can use this ruler as a flashlight. Please give me some more useful ideas
2 votes -
LinkIt ONE updates
LinkIt update requests:
-Antennas for the LinkIt to be on the board (at least the GPS). The GPS is heavy.
-Make it so that the SD card can be accessed at the same time the serial to computer is running.
-Have an external power pins for powering the unit and charging the battery.
-Move the microSD card away from the USB connection.10 votesWe’ll take all those suggestion into consideration while updating the new version. Thanks for your share.
-
stop overcharging for shipping Fusion PCBs
Please charge customers for the correct shipping weight instead of the maximum for PCBs of any given size. Most companies do this.
For an example, Arduino (shield)-sized boards are only one third the size of the 10cm x 10cm board category that must be used to buy them, but they are only ONE THIRD of the size and weight. We have to pay (express) shipping for TRIPLE the weight of the actual order and this can be substantially more expensive.
Please use the actual board size to compute the proper weight. Many other lower-cost PCB prototyping services do this, and…
23 votes -
"Service and Gifts" -> "Service" and "Gifts"
Please split the category of your shop's website for "Service and Gifts" into two categories "Service" and "Gifts". These categories have nothing to do with each other, and it makes getting to Fusion services a little more difficult.
I'm guessing that new people to the site and going to have trouble finding the PCB service ("Fusion") if they don't know that it's called "Fusion" and would not think to look in a "Gifts" category...
thanks
7 votes -
Lotus version with a Picaxe chip
The idea of combining the Grove system with an ATmega chip in the recent Lotus board is great. Working in the field of education, also using Picaxe chips along with a free flowcharting software (Logicator) we are dreaming of a same type of board with a 28x2 chip.
1 vote
- Don't see your idea?