My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
Fusion PCB Specification -- Provide separation dimensions between layers.
For computing strip-line impedance it is important to know the distance between conducting layers and the dielectric constant of the insulator material. If averages are provided please also provide variance
21 votes -
Support TI C2000 for Crazyflie
You could allow C2000 launchpad plug into actuators and sensors to control Crazyflie
1 vote -
Fix the translation for the new Mini Soldering Iron
Great product, but the translation needs some work. Here is my suggestion:
Our Mini Soldering Iron, is a small, lightweight, quick heating soldering pencil that is great for many soldering application. The stable temperature is controlled accurately by the embedded STM32 controller and is easily adjusted from 100 to 400 degrees Celsius. You will benefit from dual temperatures, accelerated sensors, included sleep mode, and automatic over-heating warning. Soldering iron tips can be replaced with 4 different types and the embedded software can be reprogramed.
Features:
Portable and lightweight for convenient soldering
Easy temperature control
Sleep mode for safety and extend…2 votes -
On the SARK-110 I would like to be able to offset the vertical axis and display the j reactive component rather than the Z impedance.
I have the SARK-110 and need to display the j component with vertical axis zero in the middle of the display. Thank you
1 vote -
Bicycle tracking and theft protection
We need a GPS device with GPRS and battery with motion charging small enough to fit inside a bicycle seat post. Or maybe fit underneath bicycle seat. When in motion it must charge the battery and transmit GPS coordinates every 30 sec via GPRS(sim card installed)
2 votes -
Give price breaks for large quantity purchase
I don't see any price breaks for large quantity orders.
10 votes -
Panelize Instruction Improvement
Improve the panelize instructions for Fusion PCB. Currently is very, very, very poor.
5 votes -
I would like to see more Grove Kits/Sensors offerings not associated with a platform. Or maybe a fill your own sensor "bag" of sensors!
I would like to see more Grove Kits/Sensors offerings not associated with a platform. Or maybe a fill your own sensor "bag" of sensors!
1 vote -
MCPCB Service request
You add a Metal Core (MCPCB) option to your already excellent Fusion service.
1 vote -
Gerber Viewer doesn't show holes.
Worried that Seeed may not see the drill files in my Gerber.
6 votes -
Fix broken EMG sensor example code!
Fix your broken EMG sensor example code. It will not compile!
1 vote -
Static URL for teachers' custom Grove starter kit
Offer pre-customized Grove Starter packs for teachers that the teacher can customize so they can give the same URL to each student so they buy exactly what they need for their class.
1 vote -
Addition of biometric scanner
Add Secugen Hamster Plus fingerprint scanner to your inventory
4 votes -
I don't see how it's possible for seeed not to see its email pictures don't download. Surely there must be some way of telling them.
I don't see how it's possible for seeed not to see its email pictures don't download. Surely there must be some way of telling them.
1 vote -
Fix the recipe interface
I have a lot of trouble getting through the recipe process.
It is extremely buggy. The ability to post formatted Arduino code to the recipe would also be nice.Maybe put a sign up to say "under construction" on this section before anyone else goes through the same pain that I just went through.
1 vote -
Create more longer cables for grove.
Create more longer cables for grove. For example 2 or 5 meters would be really useful. Thanks
9 votes -
Fusion PCB pricing
PCB should be priced by the total sq cm used & not by fixed length & width measurements. This would stop crazy price jumps. Build a board that is 5.54cm & you have to move up to 10cm size board pricing. This crazy & shouldn't be happening. Please price your boards fairer for the total area of the boards used & not for the area not used.
29 votes -
3 votes
-
I'm having communication problems
Very hard to do business with you. I'm having communication problems. I can not find contacts for communication. I do not have time. I can not spend time with you. I am in a hurry.
I canceled my order and cancel the payment.
8 votes -
Order Number: 154481
The problem is still not resolved. Waiting for your attention.
Your customer service is progressing very slowly. Problem solving long.
13 votes
- Don't see your idea?