My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
308 results found
-
Sell the matching motor separately for the Tessel Servo Module
I just ordered Tessel Servo Module 108990016
It supports multiple motors but you only sell one of this specific motor with this item. You should also sell it individually. I had to go order it from another website so that I could have 2 of the same model motors.
In fact, it would be a good upsell link like "Customers buying this also purchased..."1 vote -
Offer the 2-pin JST to JST SM cable from the EL Driver as a separate component
The Grove EL Driver comes with two cables. One of these is 2-pin JST to 2-pin JST SM for making the connection from the board to the EL Wire. My suggestion is to offer that cable as a separate item in quantities similar to those offered for Grove adapter cables.
1 vote -
Ethernet transceiver a bit noisy (but BBG is quiet in general!)
Make the ethernet transceiver radiate less. I did radiated emissions testing on the BeagleBone Green and it does quite well. It passes Class B residential, which is difficult to do. However, I had to add a ferrite on the ethernet cable. Your ethernet chip must be noisy. Thanks!
1 vote -
Bought a Grove starter kit for Arduino : poor support
I was used to working with straight forward Arduino, just fine, Thought the plug-and-play of grove was a good idea.
But the information to get it working is poor. The links on the paper do not exist anymore. No clear starting instructions what to install where exactly to get it going. Much information seems to be implicit.
Information is just not complete and/or easy to understand. Pieces are missing. You-tube?3 votes -
More information needed on out-of-stock items
More details need to be given for out-of-stock items. For example, is it being replaced? Will it be available again? When is the ETA?
For example, I have a client who needs 12 new BeagleBone Greens. They've been marked as out-of-stock for a long time now. Is this permanent? Or temporary? What do I tell my client?
13 votes -
replace generic icon with pcb render
on the account order history page pcb orders should have a rendering of the board instead of that generic icon
14 votes -
Output job file
Create output job file for use in project to generate required files in format you need. File will specify BOM format, gerber options, etc.
7 votes -
Need to improve your suppy chain
My recent order experience...
Order Number: 204016 (item in stock)
Me: 03/23/2016 - Order placed
Seeedstudio: 03/23/2016 - Order comfirmed
Seeedstudio: 03/24/2016 - Traceable; "Shipped" per your CS
DHL: 03/24/2016 - Shipment information received
DHL: 03/30/2016 - Shipment picked up
DHL: 03/31/2016 - Shipment deliveredOrder Number: 204015 (PCB)
Me: 03/23/2016 - Order placed
Seeedstudio: 03/23/2016 - Order comfirmed
Seeedstudio: 03/29/2016 - "Shipped" per your CS
Seeedstudio: 03/30/2016 - Traceable
DHL: 03/30/2016 - Tracking number not found
DHL: 03/31/2016 - Shipment information received
DHL: 04/01/2016 - No update yet...When I contacted your Customer Service on 03/29/2016, they seemed to…
1 vote -
Your web pages are difficult to follow! Difficult to determine how to get special deals, and promotions.
Make it easier to order pc boards, include discount promotions, and checking on orders purchased! You have a great company, make it easier for the USA to place orders with you. Free shipping on pcb orders would greatly increase your business!
Stephen1 vote -
Please provide support
There is no way to contact you support staff and the support button is not working. Please go out of business
2 votes -
6 votes
-
1 vote
-
Add 4x20 Grove LCD
The 2x16 Grove LCD is terrific, especially with the backlight color changes. Bring out a 4x20 version.
By the way, what are the hidden I2C addresses on this device? They should be documented so multiple devices can be used.
8 votes -
Add Mesh Support to Smart 7688 Duo
The ability to be both a Wifi station and a Wifi access point, simultaneously, would allow the Smart 7688 Duo to participate in powerful Mesh Networks. This can be accomplished virtually within a single radio (allowing for the same channel, or a more power-draining second radio). The 'hostapd' package in openwrt's Chaos Calmer supports this feature.
4 votes -
webpage inprovements
Make sure your website works with tracking instead of allways saying processing
1 vote -
DCC Stationary decoder
How to use the Arduino system as a stationary decoder for model railroad DCC. Just an article with the basic code.
1 vote -
Fix their broken website.
The Fusion PCB website is broken. It won't let me create a new account. I just get the error message "CAPTCHA Error: Session not started. The CAPTCHA cannot be used!".
I tried to report this issue through the "Contact Support" link on the feedback page but that is broken too, so this is the only way I have of reporting the issue!
1 voteYou’ll need to enable cookies on your browser (turning cookies on), try it again.
-
Email to Track and Trace number as soons as it comes available
Why I get an email to my order is traceable, but first I have to log in and go to the order history and there find the number.
Why not send the track and trace number in the email?4 votes -
Which Batteries for which product
Please specify which batteries work with RePhone and WIO - in your store, please
1 vote -
We need a MagnetoPot Potentiometer in Grove ...
http://www.spectrasymbol.com/potentiometer/magnetopots
Build us a MagnetoPot Potentiometer leaf to plug into Grove. This will allow the monitoring and response to motion using a solid state contactless sensor. These particular Pots monitor over a longer range of motion so will be highly flexible and useful in there applications for many projects and Grove user applications.3 votes
- Don't see your idea?