My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
- or
246 results found
-
Order specific communications
Add a "communications" feature in a order item that would enable sending and receiving messages that are directly linked to a specific order. In my case I wanted to send a message with some details about the PCB but it was difficult to find a way to send a message at all.
1 vote -
Accumulate Order
Your recent Flash Sales are great, but if I could pay for then combine my orders from multiple flash sales then I can save on postage costs and pay postage separately at the end. But it does mean you will need to set aside each order until the end or give buyer option.
1 vote -
not notify the customer that PCB has been shipped unless it has actually been handed over to the courier such as Fedex.
I got email from you saying my PCB has been shipped in Nov. 2. But Fedex record shows it only received it on Nov. 8, and they delivered it to me the next day, Nov 9. So there is unexplained delay of almost a week. Better to notify me the day you actually handed the PCB over to Fedex as ship date.
1 vote -
Copy of e-mail communication in order history
Since your communication e-mails gets blocked by our filters and so on, we are loosing time in orders. We placed the order and your team asked for more details. I could see reload file, but do not know what to do and I didn't realise that the email sent from your side is blocked in my side.
If you have all the e-mail records on the web side at least until the order is complete, then it will reduce delays.
Order number 190117101000
1 vote -
Thanks
Thanks for sharing so many ideas!
1 vote -
bought two new sensors and no support for GrovePi and RaspberryPi - Voltage Divider POW0516P & Temp/Humidity 101020074 need python software
Need Python test software for two new sensors, am using GrovePi and RaspberryPi. Iam sure others would like this software both very useful sensors. please update software for new sensors
Voltage Divider POW0516
Temp/Humidity 1010200741 voteThanks for your good suggestion. We’re doing.
-
Grove board for Mics 4514
Hi,
Alternatively to the Mics 2714 (recently suggested) you could produce one for the Mics 4514 which combines both nitrogen dioxide and carbon monoxide.
There is already an open HW specification with Arduino code here:
https://github.com/ShawnHymel/MICS-4514_CO_and_NOx_Sensor_BreakoutThanks!
1 vote -
feed back on web function "button"
Add a link to the footer (on all of your web pages) to "contact web support"
1 vote -
Need differntial trace width and separation for 100 ohm diif lines. Why have required order no.?
Customer Support Question should not have a required order no. field.
1 vote -
import the artificial intelligence shield for Arduino and Rasperry PI from general-vision.com
import the artificial intelligence shield for Arduino and Rasberry PI and CuriesNeurons Pro library.
1 vote -
Firefly
I wish seeedstudio would make a deal with the manufacturers of the Firefly RK-3288 and some other awesome products they are working on. Perhaps this isn't possible, but they do have some really neat things they are doing.
0 votesHi Aaron:
Thanks for your advice, we will pay close attention to Firefly RK-3288.But we don’t know the “neat things” they are doing, it will help if you can give us some info about this. -
?
customer support, when I ask a question, I want an answer, TODAY
1 vote -
A new DSO Quad
New hardware ! 4 real analog channels, 10-12 bit samples, at least 100MS/sec (per channel !). Improved "front end" and significantly more waveform memory (micro SD). Try to maintain the price point.
1 vote -
ESP8266 + SDcard + Arduino bootloader = 10$ arduino-compatible standalone datalogger
The ESP8266 can be re-flashed to allow uploading Arduino skecthes.
It also has native support for SD card.
So, a single board which includes ESP8266, an SDcard reader and battery connector would be a cool, wifi and cheap standalone datalogger (no need for external MCU).
ESP3212, just arrived to the market, even supports Bluetooth!1 vote -
Web site fix/improvements
The new user registration page is clearing the Address's State if there is an error. In my case it was the nickname. Then you get an error for that. It also forgets that you entered a captcha. You should only have to do that successfully once as you have proved you are human. There is also no indication that a Nickname needs to be unique. I would rename that Username, which is thus implied. It is also useful to use AJAX to immediately let the user know that a Username is taken, rather than waiting them to press Submit and…
1 vote -
Please fix the shop category menu (and add a shopping cart/login button to the front page)!
The Shop category menu only works for me when I'm in the shopping cart page. It doesn't work (e.g. react to the mouse in any way) on any other page of the site (using Firefox, all plugins deactivated)!
Also, the white background of the sub-menus isn't optimal in my opinion as it doesn't contrast with the white page background.
And - why is there no cart/login button on the shop page!? The only way to get there seems to be to add an item to the cart.
This is another point: I iked the old behaviour more where you were…
1 vote -
Correct your "W5500 Ethernet Shield" page
The 9th bullet point under "Features" says "Not supports IP Fragmentation". Either that was supposed to say "Now" instead of "Not" or it is worded very clumsily.
1 vote -
How about making Fusion OPL parts available for prototyping of single PCBs that I would hand solder?
Since you don't support single quantity prototypes at a reasonable cost, can you make available the OPL parts for testing on prototype PCBs that we assemble ourselves? Just allow the parts to be purchased via your Bazaar.
1 vote -
Sell the matching motor separately for the Tessel Servo Module
I just ordered Tessel Servo Module 108990016
It supports multiple motors but you only sell one of this specific motor with this item. You should also sell it individually. I had to go order it from another website so that I could have 2 of the same model motors.
In fact, it would be a good upsell link like "Customers buying this also purchased..."1 vote -
Perk up your business with CryptoPunks Clone Script
These days, CryptoPunks break the sales records among the numerous NFT projects. CryptoPunks NFT Marketplaces are proving themselves as the best digital collectibles platform by the set of desirables. If you are an entrepreneur who wants to rule the digital collectibles, this is the right time to venture into your CryptopPunks Clone by shaking hands with Maticz. Hence, acquire a huge victory in the booming NFT Sphere by getting a clasp of world-class CryptoPunks Clone Script.
Visit here: https://maticz.com/cryptopunks-clone-script
1 vote
- Don't see your idea?