more components in Open Parts Library
more components in Open Parts Library, 555, zeners, comparators, power FETs, voltage references, voltage regulators (78XXX)

-
用户
arielbmx 评论
There is not an optocoupler
-
用户
alchy 评论
CD4016BPW (LOGIC, QUAD BILATERAL SWITCH, 14TSSOP)
CD4001BPW (LOGIC, QUAD 2IN NOR GATE, 14TSSOP) and other logic gates -
用户
alchy 评论
OTA as LM13700
OPA TL072/TL074,
MCU MSP430G2553 TSSOP-28 -
用户
roland 评论
Perhaps the OPL Excel-file could have more columns like SMD/THT, Power, accuracy/tolerance, voltage
-
用户
roland 评论
I have been searching in the OPL Excel-list and I need some of the following components to be able to order soldered prototype.
The well-known 555 timer, more Zener values (3, 4.7, 5, 6.2, 8.2, 10, 12, 15, 20 Volt) and perhaps some with more power 1W, al least one comparator (LM2903, LTC1716, LTC144x, LTC184x), voltage reference (LM4120, LM4132, LT10xx, LT66xx)
FET should have low Rds(on) and if possible logic value gate threshold. But most important is low Rds(on) (CSD16570Q5B, CSD19506KCS and with dualcool csd16407q5c)
And maybe some current sense IC like INA1x9.
Perhaps a current sense resistor (LKV25R001FER)Of course it depends on what components are available for you and at what cost.
-
Thank you so much for your suggestion!
For 555, do you mean MAX1555? We have it in OPL. The SKU is 310030064.
For Zener, do you have any suggestion? How about DIP Diode 3.6V-500MW, we have it OPL. the SKU is 304030011.
For comparators, do you have any suggestion?
For FET, we have some. like N-CH 60V(305030028), P-CH 30V(305030018), do you have any specific requirement. suggestions are highly welcomed :)
For voltage references & regulators, any suggestions?