Add a DTR Pin to the dual mode Bluetooth Device so that it can also flash the microcontroller over the air.
Currently the Bluetooth Modules with HM-13 are not providing the DTR Pin that is needed to reset the microcontroller while flashing a new firmware. It would be great if that functionality could be made available on one of the programmable Output Pins.
1
vote
![](http://www.gravatar.com/avatar/613435b0321d55992de605f943a3c5e5?size=40&default=https%3A%2F%2Fassets.uvcdn.com%2Fpkg%2Fadmin%2Ficons%2Fuser_70-6bcf9e08938533adb9bac95c3e487cb2a6d4a32f890ca6fdc82e3072e0ea0368.png)
-
Neha Sharma commented
Thank you to this help