My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
Cash App Phone Number- Always ready to Support on Square
Cash App is digital payment app owned by the Square Inc. as the parent company. Cash App allows users to both transfer and receive money online. For utilizing this app it is required to create an account using a mobile number or email ID. After logging into Cash App account one can easily send or receive money. Cash App has so many great features such as free cash card, direct deposit, cash app boost, and get free money on Cash App. The direct deposit on Cash App allows users to get the paychecks directly in the bank account.
cash app…3 votes -
My Experience with The Best Online Exam Help
Since the pandemic hit us unannounced my classes were missed and no one had expected it to go this wrong. During this whole process, I was in dire need of Online Exam Help. My teachers and friends had almost given up on me. I feel lucky because I found this Online Exam Help. They were really nice to me; I would rate them a hundred over ten for the kind of professionalism that they portrayed. Not just that, they were pretty instrumental in my Statistics Case Study Assignment Help as well. I would suggest, you should get in touch with…
1 vote -
ONE SPIN casino
I played at this casino put a little more after 2k and gutted I put another 300 pounds then won a grand put for withdrawing evidence then I took note there's no british casino well it was in euros but I mean they seem to make there their own rules not enough evidence photo front back from bank card letters bank statutes and still going on this is my third attempt 5 days pass each attempt but just good that its now 1840 for withdrawing now as I hv played a little then go for withdrawing but I hope it…
1 vote -
Locksmith
Where I can find fast a car locksmith
1 vote -
Sliding patio door replacement
Hi- We're gathering info on replacing our 51 YO ten foot wide sliding patio door plus another smaller, standard size sliding door in the MBR. We want a quality door and competent installation. We had the Renewal by Andersen guy over and he left a quote for approx. $18,000 which was almost twice what we expected for the two doors. After a phone consult with the local Milgard rep, we got a quote for about $3500, which is less than half what we expected for the two doors. The Pella guy sent me an email with about 20 questions and…
1 vote -
Transportation of cars
Logistics is a rather complicated process, so I prefer to study all the information at once in order to be aware of everything that is happening in this area, I have studied all the detailed information on car transport quotes regarding transportation with help https://transportgator.com/car-transport/ , so before engaging in transportation, I suggest you get acquainted with all the subtleties.
1 vote -
A few broken chairs
I've had a few broken chairs in the last few days, it's a curse. Because of this, I have very few chairs left in the apartment and therefore I want to order new ones. Do you have any idea where I could order them from?
1 vote -
ihelpbitdefender
All in all, you should definitely go for this antivirus for security purposes. Bitdefender offers a number of features and advanced protection. It has a simplistic user interface, so it can be used efficiently. Users can either use it to fully scan their device or just a part of it.
https://ca-bitdefender.com/4 votes -
computer games
I consider computer games as much a part of our culture as television or painting. This is really a special world and I really like to do it. There are a lot of interesting things and so many different genres, it's really very exciting, isn't it?
1 vote -
instagram followers
Have you ever bought instagram followers?
1 vote -
I want to celebrate my birthday with friends
Good day to you. I want to celebrate my birthday with friends. I feel lonely. I want to make friends online. Can you share with me the best online platforms you use?
1 vote -
Late night options at online casino
At Vegas parties and online casinos, I usually leave the club around 4 or 430. I usually have to pull out of the lane to find something open. Are there any decent restaurants / eateries open around this time?
1 vote -
Online Casino
Do you play online Casino?
1 vote -
How to get rid of a problematic relationship with a girl
I'm tired of my girlfriend's disgruntled face and I want to stop dating her
1 vote -
FREE $10 no deposit at CRAZY POKER
Want $ 10 for free? Just come and play online poker at Crazy Poker!
Download our free online poker software and register a real player account, and in 5-8 hours you will have $ 5 in your poker account!
to get the remaining $ 5, just register at least one valid credit card (Visa or MasterCard). Then write to our support service and get your cash. The second $5 will be credited to your poker account within 24 hours.
It's a total of $ 10 free!
The offer is only valid for new, real players. The offer is only valid…
1 vote -
Weigthed blanket
Where can I buy a knitted weighted blanket? Those look great!
1 vote -
Identifying/Restoring old font/style?
Hello, I have been using RTSS combined with MSI Afterburner for a few years now, and I am currently running RTSS 7.2.3. I mainly only use it for FPS monitoring, using RTSS's "Show Own Statistics" feature. Up until very recently, the FPS counter was a specific font and style, shown here:
[IMG] [IMG] [IMG] [IMG]
Now, I'm not sure what changed, as I mostly left it running in the background without messing with it, but recently the style turned into this when using Vector 2D/3D:
[IMG]
The font slightly changed, and it's overall slightly squished compared to the original. It's…
1 vote -
Online relationship
Good day to you. I am 40 years old, and I want to find An Asian woman for a serious relationship. I am living in Canada, and I want to find my soul mate here. Can you help me, please?
1 vote -
How to fix up this Cash App Transfer Failed?
Most of the time, you can solve these problems yourself by following the troubleshooting tips found here. You don't need to panic if your Cash App Transfer Failed. These are some of the reasons that may be behind the failed payment of the Cash application. However, since it is used by millions of people, sometimes you may run into some problems.
https://www.apple-supportphonenumber.com/blog/why-is-my-cash-app-payment-failing1 vote -
Tips to Make Money from Satta
Something basic to know is to get the hang of everything about the delight going before placing your merited money in it. At the point when you wager for Kalyan Matka, these Kalyan Matka tips Online Casinos will help you with serving your inspiration. Get some answers concerning the redirection will help you in making more compelling technique in benefitting. Being notable about the delight will in like manner give you better choice of where absolutely to bet. To benefit in wagering, one requirement to give time and dedication in making wagering aptitudes. Furthermore, encountering some wagering rules will similarly…
1 vote
- Don't see your idea?