My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
- or
No existing idea results
- ~ No ideas found ~
554 results found
-
Live chat
Live chat. Response rate to messages sent is very slow
5 votes -
1 vote
-
Release 3D-files for Wio link, Wio node and compatible grove sensors to make it easier for users to create their own 3D-printable casings
Release 3D-files for Wio link, Wio node and compatible grove sensors to make it easier for users to create their own 3D-printable casings and holders.
4 votes -
E-Test: where to order?
Hello, I am looking for a manufacturer of PCBs. I found somewhere that I can order 100% E-Test for 10$, but where do I select it?
Cheers, Sebastian1 vote -
Kicad lib for OPL
Create an OPL lib for Kicad
13 votes -
+One Button "Please get this in stock"
+One Button "Please get this in stock" request - to indicate how large the interest is in a product.
2 votes -
AC Voltage Measurement Sensor
I would like to be able to read the ac voltage upto 250 VAC and pass the value to an MCU such as an Arduino or Raspberry Pi. I suggest that an analog value between 0-1023 (5VDC) would be suitable.
I cannot see why this cannot be done as I see almost throw away measurement devices with an LCD screen. I just want the raw data without a screen.
An ability to also obtain amps and hertz either as a consolidated sensor or 3 separate sensors would be even better.
Thank you5 votes -
Add order status in the order information.
Add the order status in the order detail information.
2 votes -
Bought a Grove starter kit for Arduino : poor support
I was used to working with straight forward Arduino, just fine, Thought the plug-and-play of grove was a good idea.
But the information to get it working is poor. The links on the paper do not exist anymore. No clear starting instructions what to install where exactly to get it going. Much information seems to be implicit.
Information is just not complete and/or easy to understand. Pieces are missing. You-tube?3 votes -
bad service
Order Number: 185250 not delivered. SG post not showing tracking anymore. Has been 3mths and local PO says has been returned to sender. Support not answering emails. Pls refund
8 votes -
2 votes
-
BT blink sound for bikes
Needed a simple beep or sound generator and a bluetooth sending device with a common BT protocol in a water resistant housing on base of 12 V and a trigger input (or two).
The trigger could be connected with the blinking relais, controling light or the two blinking lights.-> EASY, SIMPLE but VERY valuable for bikers, because they could hear the blinking INSIDE the helmet, while OUTSIDE beepers are forbidden for being too loud for the surrounding to be heard inside the helmet while cruising fast speed.
I think this gadget should be sold very often, because its very cheap to built and easy to implement into the bike by nearly everybody. On the other hand practically very interessant for every biker.
Yours
PeterNeeded a simple beep or sound generator and a bluetooth sending device with a common BT protocol in a water resistant housing on base of 12 V and a trigger input (or two).
The trigger could be connected with the blinking relais, controling light or the two blinking lights.-> EASY, SIMPLE but VERY valuable for bikers, because they could hear the blinking INSIDE the helmet, while OUTSIDE beepers are forbidden for being too loud for the surrounding to be heard inside the helmet while cruising fast speed.
I think this gadget should be sold very often, because its very…3 votes -
ADDA
I've tested succesfully ADDA using only a tester, no oscilloscope or logic analyzer. These are my results: easy enough for the first steps.
I tested only A/D.
regards
Trevisan Andrea1 vote -
Which Batteries for which product
Please specify which batteries work with RePhone and WIO - in your store, please
1 vote -
Better inventory management needed
Most products that I would to order are out of stock! :( Water pump, relay, flow sensor, etc. There should be an option for back-order or notification to customer when the product is back in stock.
8 votes -
6-layer boards, 35\my\ on inner layers, metal-filled vias, "0.1500".
Indeed 4 points...
1) 6-layer boards
On my WishList I have 6-layer boards.
2)
Another point is 35\my\ of coippeer on inner layers
3)
The option to have vias or holes in SMD pads metal-filled (as some PCB manufacturers offer). Or the simplified "poor-mans method" to add a third solder-mask which just adds "lids" over the holes on top or bottom side; controlled with an additional "Via Key" layer.A "SMD pad with a hole" is a pad defined as a through-hole with the top-layer shape the shape of "the same" SMD pad, a circular shape in other layers.
4)
How difficult would it be to make traces, annulars etc. 0.1500mm, today's lower limit 0.1524mm (6 mils)?Generally speaking, I see you with your pricing as the "final resource" for the Hobbyist. Definitely realistic for the Hobbyist to make a good PCB instead of "messing with" primitive lab boards, etc.
/dindea (Staffan Cronstrom)
Indeed 4 points...
1) 6-layer boards
On my WishList I have 6-layer boards.
2)
Another point is 35\my\ of coippeer on inner layers
3)
The option to have vias or holes in SMD pads metal-filled (as some PCB manufacturers offer). Or the simplified "poor-mans method" to add a third solder-mask which just adds "lids" over the holes on top or bottom side; controlled with an additional "Via Key" layer.A "SMD pad with a hole" is a pad defined as a through-hole with the top-layer shape the shape of "the same" SMD pad, a circular shape in other layers.
4)
How…7 votes -
Fusion PCB Specification -- Provide separation dimensions between layers.
For computing strip-line impedance it is important to know the distance between conducting layers and the dielectric constant of the insulator material. If averages are provided please also provide variance
21 votes -
talk to phone to enter nos only
e-ink display is what we need for sunlight readability
1 vote -
A lot of products with Seeedday coupon are not in stock or discontinued. Very annoying!
A lot of products with Seeedday coupon are not in stock or discontinued. Very annoying!
7 votes -
Update the WIKI
New products or new versions of products, Grove Temp sensor V1.2, could not find it. Many bad links. Kit products with new version of hardware but wiki goes to old version of the product. Grove Starter Kit for Arduino V3 has some in it. New products or versions of products in the store going to old versions on wiki. I think the store and the wiki could use a good going over and clean up.
7 votes
- Don't see your idea?