6-layer boards, 35\my\ on inner layers, metal-filled vias, "0.1500".
Indeed 4 points...
1) 6-layer boards
On my WishList I have 6-layer boards.
2)
Another point is 35\my\ of coippeer on inner layers
3)
The option to have vias or holes in SMD pads metal-filled (as some PCB manufacturers offer). Or the simplified "poor-mans method" to add a third solder-mask which just adds "lids" over the holes on top or bottom side; controlled with an additional "Via Key" layer.A "SMD pad with a hole" is a pad defined as a through-hole with the top-layer shape the shape of "the same" SMD pad, a circular shape in other layers.
4)
How difficult would it be to make traces, annulars etc. 0.1500mm, today's lower limit 0.1524mm (6 mils)?
Generally speaking, I see you with your pricing as the "final resource" for the Hobbyist. Definitely realistic for the Hobbyist to make a good PCB instead of "messing with" primitive lab boards, etc.
/dindea (Staffan Cronstrom)
![](http://www.gravatar.com/avatar/7d903aaff8daac55bd8da3e729d2188f?size=40&default=https%3A%2F%2Fassets.uvcdn.com%2Fpkg%2Fadmin%2Ficons%2Fuser_70-6bcf9e08938533adb9bac95c3e487cb2a6d4a32f890ca6fdc82e3072e0ea0368.png)