My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
- or
554 results found
-
Raspberry Pi support for Grove-TF Mini LiDAR
Raspberry Pi support for Grove-TF Mini LiDAR
1 vote -
0.4mm rigid boards
0.4mm rigid boards as standard choice
1 vote -
1 vote
-
Soldering stainless steel to PCB
How can you bond a delicate PCB with a stainless steel component?
http://www.superiorflux.com/soldering-stainless-steel-components-pcb/
1 vote -
received
Please check your shipping records, because I already received the rock960 board.
1 vote -
Account management
Don't add additional accounts automatically from PayPal payments - use the customer selected/created account
1 vote -
Accept Octopart links rather than specific vendor links
In a BOM, accept Octopart references rather than specific part + vendor. This gives everyone the most flexibility.
1 vote -
Control level
Control water level of some tanks in a farm at 1.5 km distance from the main house.
1 vote -
Add STM8S003F3 to component list
It is the lowest cost and most commonly used MCU.
Can be programmed using the high speed and cheap ST-Link.
1 vote -
Only let an order be placed if the necessary files are uploaded
I've had it many times that the board outline hasn't been provided, even when it had. It would be nice for the site to tell me that there is a problem so I can fix it there and then rather than wait for my order to be rejected.
3 votes -
reduce the shipping costs to max 10% of the price
Shipping costs at Fedex being around 1/2 of the items prize + customs 1/2 of the items price doubles the price. I'm refusing to pay the customs fee, as this wasn't mentioned in any of your emails or on the order forms.
1 vote -
Fusion BOM upload error list
I am trying to upload a BOM for fusion with about 25 items. The upload keeps providing errors, and I can't find the mistake. Please list the errors, when the BOM does not conform.
1 vote -
PCB with 3mil trace
hi,
I have track width of 3mil.
How to proceed for that order1 vote -
Shipping quote
Include shipping information in the online quote.
1 vote -
Check the FPC specifications.
Currently the Fusion PCB Specifications page says that FPC can do 0.1mm track width and track spacing (ie 4 mil). However, when ordering an FPC the only selectable track width/spacing is 6 mil. One of these must be wrong!
1 vote -
RAM ddr3 1-2 GB (with same phisical as today)
what kind of application runs on 128mb today??
RAM DDR3 1 - 2 GB !!just RAM.
(phisical today was already good, as small as possible with sdcard)1 vote -
Seeed studios should take care for fusion service which is not trustable. you just order, pay, and wait forever
Seeed studios should take care for fusion service which is not trustable. you just order, pay, and wait forever for your orders
1 vote -
Reply to ALL Emails
Reply to all the emails. I sent an email to Molly but hasn't received a reply.
1 vote -
Why donot you answer my questions I post
I wrote several mails and complains. why you do not answer me. it is a very simple question. what is my correct tracking number what is the tracking link and where is my parcel now.
1 vote -
DipTrace gerber export tutorial incorrect (twice)
In your tutorial regarding how to export gerber files from DipTrace, you show the resulting output files as all having .gbr extension, yet your standard is for the extension to indicate the type of file and for each file name (sans extension) to be the same. That is misleading.
Also, you show a set of Gerber file types highlighted in the Layers box. This will NOT limit the output to only those file types. When you hit the "Export All" button it will, literally, Export ALL of the file types, not just the ones that were highlighted.
There is a way to get the DipTrace Gerber Exporter to export the files in the way SeeedStudios requires:
- Click on the "Files" button.
- Under the Filename column, enter "<project>.ext". Don't include the quotes and replace "ext" with the proper extension for that file type. For instance: for "Top Silk" enter "<project>.GTO". For "Top Mask" enter <project>.GTS.
- Under the 'Include into "Export All"' column, set to "yes" all of the files SeedStudios requires, and "no" for all other file types.
- Click "OK"
Once this is set up, hitting the "Export All" button will format the filenames in the SeeedStudio style AND will only export the file types that SeeedStudio requires. BTW: the "<project>" field is replaced with the project name, thus, each output file will have the project name as the body (with the appropriate extension).
In your tutorial regarding how to export gerber files from DipTrace, you show the resulting output files as all having .gbr extension, yet your standard is for the extension to indicate the type of file and for each file name (sans extension) to be the same. That is misleading.
Also, you show a set of Gerber file types highlighted in the Layers box. This will NOT limit the output to only those file types. When you hit the "Export All" button it will, literally, Export ALL of the file types, not just the ones that were highlighted.
There is a…
3 votes
- Don't see your idea?