My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
- or
246 results found
-
Secure the checkout/payments page please
Please make your checkout / payments page fully secure. I had to cancel my order since I was not going to enter my CC details when both Firefox and Chrome inform me the page is not fully secure.
1 vote -
Support TI C2000 for Crazyflie
You could allow C2000 launchpad plug into actuators and sensors to control Crazyflie
1 vote -
1 vote
-
1 vote
-
I'm having communication problems
Order Number: 154481
Please cancel my order. Please refund my money. Because we are experiencing communication problems. I've got to hurry. I need to urgently Manufacturers of PCBs. But a little problem takes days I ask you your fix. Five days still not started to manufacture PCBs.1 vote -
UPS board for generic SBC
There are few boards with native lithium battery support but it would be nice to add UPS like function to any 5V powered board, be it ARM or Atmel. AXP209 is integrated on some boards and I believe it would be very interesting to have it on a breakout board similar with a solar charge controller. The simplest configuration would have only 6 pins (5V--In&GND / Batt+&Batt- / 5V-Out&GND). Some extra feature would make it even better: an EN pin that would cut-off both battery and Vin input. An AO pin to measure the battery voltage, a DO to send…
3 votes -
A UMTS compatible version of the phone module would be great. RePhone is GSM only. I need UMTS/AWS for ,my cell provider.
Either the main cellular module or an add-on board that is UMTS/AWS.
1 vote -
ESPxx modules would be much better with onboard microsd reader.
ESP8266 and ESp3212 are great... but why aren't they equipped with a microSD card reader, which is natively supported by the ESPxx?
2 votes -
Fix the translation for the new Mini Soldering Iron
Great product, but the translation needs some work. Here is my suggestion:
Our Mini Soldering Iron, is a small, lightweight, quick heating soldering pencil that is great for many soldering application. The stable temperature is controlled accurately by the embedded STM32 controller and is easily adjusted from 100 to 400 degrees Celsius. You will benefit from dual temperatures, accelerated sensors, included sleep mode, and automatic over-heating warning. Soldering iron tips can be replaced with 4 different types and the embedded software can be reprogramed.
Features:
Portable and lightweight for convenient soldering
Easy temperature control
Sleep mode for safety and extend…2 votes -
I want to pay extra for options
Dear, I want to pay USD 10 for my PCB project extra because of panel. How can I do this?
1 vote -
add user reference
Would be good to be able to enter a user reference when ordering PCBs. It's often difficult to know what boards my orders correspond to.
1 vote -
Single board computer with embedded 3g modem
I just saw the RePhone and the Linkit One, but these are powered by microcontrollers, why not develop a single board computer like the Beaglebone green or Raspberry Pi but with an embedded 3G modem and LiPo battery support
2 votes -
1 vote
-
Add button to change order status in order history
In my order history I have several order marked as "Traceable" but I receive the order.
Add a user button to change the status to "Finisced"
1 vote -
Inovoice address
Please do not mix shipping and billing address. For my order, i always get Billing and address are SAME though i mention clearly shipping and billing are different.
1 vote -
How about including the file name information on the ORDERED screen so that customers can see what they have actually placed an order for.
How about including the file name information on the ORDERED screen so that customers can see what they have actually placed an order for.
I currently have a multiple order in place, with more boards required.
My problem is that I can not see which boards "names" are currently in the queue and I therefore have to wait until all of the boards have arrived here "at home base" tobefore I can place my next order.
Thanks.1 vote -
ADDA
I've tested succesfully ADDA using only a tester, no oscilloscope or logic analyzer. These are my results: easy enough for the first steps.
I tested only A/D.
regards
Trevisan Andrea1 vote -
How about data on the Edsion Xadow product such as why things are not working? Also a test to tell you the thing is working? Flashing light.
Flasing lights don't anwer the question if the system is working? The OLED pretty much should have some indication there is power ? Nothing!! My only guess is the thing is bad from out of the box.
1 vote -
Mobile site displays incorrectly
On my moto G3, the mobile site displays incorrectly. There is a big white box over the majority of the text, and the font is too small for this screen.
I sometimes wonder why bother making a mobile site when it's just rubbish?
1 vote -
Order specific communications
Add a "communications" feature in a order item that would enable sending and receiving messages that are directly linked to a specific order. In my case I wanted to send a message with some details about the PCB but it was difficult to find a way to send a message at all.
1 vote
- Don't see your idea?