My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
147 results found
-
Optoisolator
I wish that in the OPL parts, you can find a place also for an optoisolator like the PC817. This is a good component when we need to make a strong separation between different supplies. Especially for microcontroller!
10 votes -
more components in Open Parts Library
more components in Open Parts Library, 555, zeners, comparators, power FETs, voltage references, voltage regulators (78XXX)
16 votes -
Max485
I wish to have in your OPL list the posibility to use the well common MAX485. When I develop boards with Modbus communication feature, I always need to use this components.
Thanks9 votes -
I would to see a GPS Bee with a backup battery. So far every start is a cold start.
I would love to see a GPS Bee with a backup battery. So far every start is a cold start.
1 vote -
don't ask for password as guest
I'm trying to check out as a guest, but the form won't let me continue without entering account details (password) to create an account.
If that's compulsory, don't offer guest checkout, as that clearly doesn't exist now.7 votes -
Pay direct via QIWI or Yandex money.
It will be very simple to pay from Russia!
4 votes -
I do not get response and I need to RMA a non-working LinkitOne
I wish I could get a response to the two messages related to needing to RMA a non-working LinkitOne I received
1 vote -
bought two new sensors and no support for GrovePi and RaspberryPi - Voltage Divider POW0516P & Temp/Humidity 101020074 need python software
Need Python test software for two new sensors, am using GrovePi and RaspberryPi. Iam sure others would like this software both very useful sensors. please update software for new sensors
Voltage Divider POW0516
Temp/Humidity 1010200741 voteThanks for your good suggestion. We’re doing.
-
3G support for Linkit One/Linkit A-Core
3G support for Linkit One
3 votes -
you have clock in your web when your time, thanks
for discount internationals
3 votes -
create a vacuum / pressure sensor from 30" Hg to 3 atm.
A vacuum and pressure sensor that is Arduino compatible that can measure from 30" mercury vacuum to approximately 3 atmospheres pressure. It'd be great for those of us using Arduino as engine ECUs to be able to have fine-grained control of engine parameters by knowing intake vacuum or pressure. Knowing the intake cross-sectional volume, the intake vacuum or pressure (in the case of blown engines) could also be used as an intake air flow sensor, which will really be beneficial to those of us using heated water injection to create extra cylinder pressure via steam expansion (to measure if we're…
3 votesHi DB:
We think this is a very professional area for the industrial control, would you please give us more advise about the popular sensors in this area, so we can make our products more convenient for you to use. -
support question
Hello Support Team,
I got a tick tock shield for my daughter, but now I realize we are missing some parts (see below), I would like to add them from german retailers, can you provide me with the specifications?
Thanks, best regards, Andreas
[email protected]
Thermistor RT1 1
Light dependent resistor LDR1
Crystal X1the capacitors are described well enough in the soldering guide
1 vote -
Screw Shield Board for Industrial DIN Rail Enclosures
Seeeduino and Linkit can replace and disrupt industrial PLCs industry. Your boards only need a Screw Shield with 5.08mm pitch screws and a screw shield PCB so it can fit in traditional Bud Industries industrial enclosures (those enclosures are very inexpensive).
So the screw shield should meet Arduino connector specs and also needs the PCB to be sized such way that fits perfect inside the enclosure.
Please see the PCB board currently offered by BudIndustries, which can be easily adapted to work like a screw shield for seeeduino platform.
Yes, the Seeeduino ScrewShield will be bigger but will provide space…
1 vote -
Tutorials
Tutorials for how to use your shields would be great. Especially configuring other devices that run off of them. Like an X-Bee for example
0 votes -
Support ODB++ file format
It would be very nice if you could handle ODB++ format also.
From my point of view, it is very easy to work with. After "I saw the light" with this format (compared to gerber), I prefer not to use gerber.5 votes -
Fix the responsive layout on windows
you could tweak your responsive breakpoints.
It's great that the site scales and works on mobile :D
But on windows, the layout hasn't taken into account the fact that scrollbars take up some of the reported available screen width.
With my 1200px wide monitor, this causes an unneccessary horizontal scrollbar.
3 votesHi Stian, thanks for your helpful information. We’ve started fixing it.
Thanks again and have a great day. -
0.4mm rigid boards
0.4mm rigid boards as standard choice
1 vote -
1 vote
-
Control level
Control water level of some tanks in a farm at 1.5 km distance from the main house.
1 vote -
PCB with 3mil trace
hi,
I have track width of 3mil.
How to proceed for that order1 vote
- Don't see your idea?