My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
147 results found
-
e-ink or oled starter kit
arduino to make mimi bt display unit and connect to mobile
1 vote -
wonder if seeed has anything that could send an sms when the diaper is wet ;)
wonder if seeed has anything that could send an sms when the diaper is wet ;)
1 vote -
Official Raspberry Pi Touchscreen - Power bridge
Official touchscreen has a long jumper cable for power.
This can be much nicer with two small PCBs.
There may also be a micro-usb connector for the power supply.1 vote -
A new DSO Quad
New hardware ! 4 real analog channels, 10-12 bit samples, at least 100MS/sec (per channel !). Improved "front end" and significantly more waveform memory (micro SD). Try to maintain the price point.
1 vote -
I want to pay extra for options
Dear, I want to pay USD 10 for my PCB project extra because of panel. How can I do this?
1 vote -
Linkit Assist 2502 Wiki and Projects
Complete support and Wiki page for Linkit Assist 2502. It says it works with xadow but nothing is clear in the manual provided by mediatek and not even a single project image or video on the internet. Makes me skeptical whether to buy the kit or not because after buying it, I won't be able to know how to handle it.
1 vote -
Accumulate Order
Your recent Flash Sales are great, but if I could pay for then combine my orders from multiple flash sales then I can save on postage costs and pay postage separately at the end. But it does mean you will need to set aside each order until the end or give buyer option.
1 vote -
Adapter Boards
I would like to be able to put smaller pitch components onto a regular breadboard.
Currently I have a number of leads from a mother board that fit very small pitch connectors. I need to be able to breakout these headers to fit onto a regular breadboard.
I cannot even find prototype boards with other than 2.54 pitch holes, let alone a dual size board.
Adapter boards that allow a dual row small pitch header to be fitted that breakout to standard size would be great. Currently I have 16 pin, 8 pin and 6 pin dual row headers that…1 vote -
new customer
set terms with seedstudio to make purchases
1 vote -
Tech Support Page Not Working
I noticed that when I enter information on the tech support page that I get error 405 - Not allowed.
Can you please fix that problem?
1 vote -
Adapt your code for RGB matrix ?
Hi,
I need a pilot board for a 64x32 RGB Leb Matrix. I saw your matrix driver board here : http://www.seeedstudio.com/item_detail.html?p_id=2645
But it doesn't seem to pilot RGB matrix... only RED and GREEN matrix. Is it possible to adapt the code for this ?
Thanks,
Mike
1 vote -
"Processing" is not a very descriptive way of telling me where my project is at.
I can't see any deeper information than that my project is "processing" what does this mean? When can I expect it to change?
1 vote -
Electrical Conductivity Sensor
It seems to me like the only thing you guys are missing for building a hydroponics environment monitor with Grove is the Electrical Conductivity sensor. I'm working on building such a monitor and it'd be great to use Grove for it :)
1 vote -
Create some nordic semiconductor nrf52 board.
Some small beacon-like nrf52 board. Like armstart one for nrf51
1 vote -
Can you make the LinkIt 7688 with more flash memory? There is not a lot of space for software. Less RAM would not be a problem.
Can you make the LinkIt 7688 with more flash memory? There is not a lot of space for software. Less RAM would not be a problem
1 vote -
new connectors needed
flat cable 2x40 pins low cost IDE specs
connector male IDE 2x40 specs, to construct flat cable connection
to mate with Mega edge connector
connector 2x8 female IDE connector for flat cablesmale connectors and male pins to construct Grove connector
RC plane (yes airplane) LI-PO battery connectors male females with male/females pins to construct longer cable connection
ONE to Many connector like 2- input female pins to insert to connector with connector other side has 8 output to insert male or female pins, called distribution connector, just like the black 0.1"(2.54mm) crimp connector.
this connector does not exists yet…1 vote -
home production
need bulk discount , for like 50-1000 pcs that should cost near about production cost .
it is not possible to solder this chips at home.1 vote -
20x4 LCD Module for raspberry pi zero
just like this seeedstudio product
https://www.seeedstudio.com/Raspberry-Pi-RGB1602-LCD-Module-p-2803.html
but for 20x4 LCD Module for raspberry pi zero. all electronics and buttons should be on the back of shield, so it looks clean.1 vote -
1 vote
-
A relay shield with Capacitor on each that can be adjusted. as well as a potentiometer
A relay shield with Capacitor on each that can be adjusted. as well as a pot on each.also an ferrouse metal sleeve where you tie in the leads to keep the power from to stablize voltage. We also need a singing tesla coil wireless power transfer shield. hell even if its just for the crazy texan
1 vote
- Don't see your idea?