My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
147 results found
-
Please block your google ads from displaying on hate website Breitbart News
A simple way to resist Trump's attack on science is to defund the hate website breitbart.com
Please block your google ads from displaying on hate website Breitbart News. #madblock
4 votes -
Support nicknames for accounts in the Fusion gallery
At the moment the Fusion Gallery shows my real name. I'd prefer to use an alias, a nickname. Allowing nicknames would encourage me to share more projects.
3 votes -
Support Target3001 files
Support Target3001 Files
3 votes -
Test Your Webpage
For years everything worked seamlessly but now the webpage is full of bugs. Next to the user icon it shows "Hi,?????". Trying to order a Fusion PCB with Firefox everything works, except the "Add to Cart" button does nothing, I tried with 2 versions of FF. With Chromium the menu doesn't work, nothing happens if I move the mouse pointer to the "Fusion" menu. Pressing the mouse button opens the menu, but releasing it goes to a different page. Some links give a 504 error. My address book is empty and all old orders are gone too.
Please install a…3 votes -
please provide student discount on the devices
please include student discount for the student buyers
3 votes -
GSM for Pebble
Can we connect the GSM module to Pebble? because I want to leave my phone :), I wait for your comments.
3 votes -
3 votes
-
USB or Grove barcode readers
Need some USB or Grove barcode readers that can be used with BeagleBoneGreen.
3 votes -
Plase fix the shopping cart!
In an earlier step I added an item to the shopping cart which I now don't need anymore.
But there is no function to remove an item: no "remove" link and button "-" only reduces count down to "1" but not to "0".
Please fix this asap, as I cannot order anything by now without also ordering the superfluous item.
Second, you suggest to go to shopping cart and use the link "estimate shipping costs" if you want to know how much shipping will cost before checkout ... Nice! But there is no such link!
3 votes -
Accurate shipping price evaluation (include import taxes for UPS/DHL/...)
I bought 10 PCB for 4€38 - 1€32 discount. (round to 4$).
I payed 21€38 shippement (round to 25$) using UPS.
So far so good, this was calculated and announced.
BUT I had to pay additional 20€ to UPS (round to 25$) (about 5€ VAT + 15€ fees for UPS ! )This fees are precisely calculated and could be known in advance, please include them (even just estimation) in cart page.
Simple first step could be to put a simple warning.PS: I do not even know how seeed earn money with such low prices
3 votes -
Liquid density and temperature sensor (sterilizable)
An addressable, 1 or 2-wire protocol reporting sensor that, when placed in a liquid could report on the temperature and density of that liquid.
This sensor could be used to determine specific gravity during brewing etc.
Also, as a secondary wish - adding a pH sensor would be awesome.
3 votes -
Full View of Check Out Cart
Being able to scroll through the full list of items in the cart when clicking the cart icon.
3 votes -
you have clock in your web when your time, thanks
for discount internationals
3 votes -
create a vacuum / pressure sensor from 30" Hg to 3 atm.
A vacuum and pressure sensor that is Arduino compatible that can measure from 30" mercury vacuum to approximately 3 atmospheres pressure. It'd be great for those of us using Arduino as engine ECUs to be able to have fine-grained control of engine parameters by knowing intake vacuum or pressure. Knowing the intake cross-sectional volume, the intake vacuum or pressure (in the case of blown engines) could also be used as an intake air flow sensor, which will really be beneficial to those of us using heated water injection to create extra cylinder pressure via steam expansion (to measure if we're…
3 votesHi DB:
We think this is a very professional area for the industrial control, would you please give us more advise about the popular sensors in this area, so we can make our products more convenient for you to use. -
No pagination would be great, instead use "infinite" scroll
I really don't like browsing in paginated overview pages
3 votes -
Product Idea
Hologram's Dash IoT product
3 votes -
Correct your weeb page
http://www.seeedstudio.com/service/index.php?r=pcb&ref=banner_fusion_fusion201631
in this page it says 4.9$ for 10 pcs but when you click it it changes to $9.9
why it is different ?3 votes -
Wireless charging for Super Capacitor
A wireless charger that can charge a Super Capacitor [SC]. It would have an adjustable maximum voltage of 2.0 to 2.5 volts, and be able to dump large amounts of current [5A or more -- much more] into an extremely low impedance load [i.e. a current source with an upper voltage limit]. Also, it should be able to dump current into the SC at full bore all the way up to the maximum voltage. A typical SC has a maximum voltage of 2.7 volts, but should not be charged higher than around 2.2 to 2.5 volts [the higher the voltage…
3 votes -
change settings of an order
on order nummer 170406231014 can i change the dimension in 100mm?*70mm?
and Layer into 1 and PCB color in blue ?
I have doing to wrong by doing first the setting and then upload the file.regards ronald
3 votes -
India
I wish we, the makers/enthusiast from India, can buy directly or from official affordable resellers from India. We are paying arm and leg, also the availability is less than the availability of the Unicorn.
Please have some affordable shipping for India or setup a sales channel/warehouse/official resellers.
3 votes
- Don't see your idea?