My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
Shipping needs major work
I had known it would take almost a week to send my order i would have ordered elsewhere.
6 votes -
Add back facebook login
I use to login with facebook and order several orders. But I cannot do it with new website
6 votes -
Better Delivery Dates!!! It's been two weeks and still nothing and no status changes.
Speed up the delivery times. 13 days in the "Processing" status, is a little ridiculous with no updated status or Estimated Delivery Date. No information at all.
What is going on with my order? Is there a problem? Should it take 13 days in "processing"?
Thanks,
Larry6 votes -
Support ODB++ file format
It would be very nice if you could handle ODB++ format also.
From my point of view, it is very easy to work with. After "I saw the light" with this format (compared to gerber), I prefer not to use gerber.5 votes -
Sensor board, or arduino shield, based on the AS3935 chip
The AS3935 has a very sensitive lightning detector with SPI and I2C interfaces and needs only a few other parts. Putting this chip on a sensor or shield would make it very easy to build an Arduino lightning detector that could count lightning strikes, log them, and warn of a coming lightning storm. Would be great for a weather station project too.
5 votes -
Customer dissatisfaction
I can not reply to posts. I will tell my forum this subject countries. http://www.picproje.org
I said you're a reliable company. Because you do not take into account the customer. You do not give value. Five days I'm struggling on you.
5 votes -
Create a board like the BBG but without any connectors
There are so few companies that are making modules like the BBB/BBG without the ethernet & USB connectors. This is an embedded market product so lets make it that way. I want to plug the module into my circuit board and put the connectors where I need them to be.
5 votes -
AC Voltage Measurement Sensor
I would like to be able to read the ac voltage upto 250 VAC and pass the value to an MCU such as an Arduino or Raspberry Pi. I suggest that an analog value between 0-1023 (5VDC) would be suitable.
I cannot see why this cannot be done as I see almost throw away measurement devices with an LCD screen. I just want the raw data without a screen.
An ability to also obtain amps and hertz either as a consolidated sensor or 3 separate sensors would be even better.
Thank you5 votes -
eC compitable stencil and PCB, and visual check tool like Eurocircuits have
Can you add the option (like on the Eurocircuits website) to make PCB and stencil compatible with the eC standard?
Eurocircuits is a European PCB manufacturer, they sell a common used stencil machine the eC-stencil-mate:
http://www.eurocircuits.com/ec-equipment-ec-stencil-mate/
The eC standard can be found here:
http://www.eurocircuits.com/ec-registration-system/
Here you can find the option:
http://be.eurocircuits.com/shop/orders/configurator.aspx
eC-registration compatible PCBIt is also recommended to make a visual check tool, such as Eurocircuits have.
5 votes -
cancel or change the order while it is in processing status
Can you offer the possibility to cancel or change an order while it is in processing status please ?
5 votes -
kit to connect notebook LCD lvds type pinout to arduino or raspberry pi and others
Kit to connect several lvds LCD types to projects and signal search. To notebooks older, the lcd lvds can be recycled to projects with arduino and raspberry pi or other connections computers's.
4 votes -
Pay direct via QIWI or Yandex money.
It will be very simple to pay from Russia!
4 votes -
Your online BOM List can not be filled. Please fix it.
Bom list can not be filled online. Online list does't show.
4 votes -
Need to know if there is free shipping to Beijing
I urgently need to know if there is any free shipping to Beijing area.
Also Transit time and if there is no free shipping then cost to shipping Beijing.
4 votes -
Provide CAD files in KiCAD
Would be good if current CAD files be offered in KiCAD rather than Eagle format
4 votes -
Output Job Flie for Altium who ganerate the Gerberfiles
Output Job Flie for Altium who ganerate the Gerberfiles so everithing is setup correctly for PCB Produktion including the correct milling Layer
4 votes -
Orange Color PCB
I'd like the color orange added for the solder mask.
Thanks
4 votes -
Please block your google ads from displaying on hate website Breitbart News
A simple way to resist Trump's attack on science is to defund the hate website breitbart.com
Please block your google ads from displaying on hate website Breitbart News. #madblock
4 votes -
Extension Cable for Grove
I wish there was a male-female Grove cable with, let's say, 100 cm as a extesion cable. Alternatively a tiny male-male PCB could act as an "extension adapter".
4 votes -
Are you planning to sell something using nrf52840 (raytac MDBT50_module for example)?
To use some module with nrf52840
4 votes
- Don't see your idea?