My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
Tutorials
Tutorials for how to use your shields would be great. Especially configuring other devices that run off of them. Like an X-Bee for example
0 votes -
create a vacuum / pressure sensor from 30" Hg to 3 atm.
A vacuum and pressure sensor that is Arduino compatible that can measure from 30" mercury vacuum to approximately 3 atmospheres pressure. It'd be great for those of us using Arduino as engine ECUs to be able to have fine-grained control of engine parameters by knowing intake vacuum or pressure. Knowing the intake cross-sectional volume, the intake vacuum or pressure (in the case of blown engines) could also be used as an intake air flow sensor, which will really be beneficial to those of us using heated water injection to create extra cylinder pressure via steam expansion (to measure if we're…
3 votesHi DB:
We think this is a very professional area for the industrial control, would you please give us more advise about the popular sensors in this area, so we can make our products more convenient for you to use. -
Screw Shield Board for Industrial DIN Rail Enclosures
Seeeduino and Linkit can replace and disrupt industrial PLCs industry. Your boards only need a Screw Shield with 5.08mm pitch screws and a screw shield PCB so it can fit in traditional Bud Industries industrial enclosures (those enclosures are very inexpensive).
So the screw shield should meet Arduino connector specs and also needs the PCB to be sized such way that fits perfect inside the enclosure.
Please see the PCB board currently offered by BudIndustries, which can be easily adapted to work like a screw shield for seeeduino platform.
Yes, the Seeeduino ScrewShield will be bigger but will provide space…
1 vote -
Sensor board, or arduino shield, based on the AS3935 chip
The AS3935 has a very sensitive lightning detector with SPI and I2C interfaces and needs only a few other parts. Putting this chip on a sensor or shield would make it very easy to build an Arduino lightning detector that could count lightning strikes, log them, and warn of a coming lightning storm. Would be great for a weather station project too.
5 votes -
kit to connect notebook LCD lvds type pinout to arduino or raspberry pi and others
Kit to connect several lvds LCD types to projects and signal search. To notebooks older, the lcd lvds can be recycled to projects with arduino and raspberry pi or other connections computers's.
4 votes -
Support ODB++ file format
It would be very nice if you could handle ODB++ format also.
From my point of view, it is very easy to work with. After "I saw the light" with this format (compared to gerber), I prefer not to use gerber.5 votes -
Fix the responsive layout on windows
you could tweak your responsive breakpoints.
It's great that the site scales and works on mobile :D
But on windows, the layout hasn't taken into account the fact that scrollbars take up some of the reported available screen width.
With my 1200px wide monitor, this causes an unneccessary horizontal scrollbar.
3 votesHi Stian, thanks for your helpful information. We’ve started fixing it.
Thanks again and have a great day.
- Don't see your idea?