My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
add re order tap to PCB order history (ie as it was).
add re order tap to PCB order history (ie as it was).
2 votes -
Tech Support Page Not Working
I noticed that when I enter information on the tech support page that I get error 405 - Not allowed.
Can you please fix that problem?
1 vote -
new customer
set terms with seedstudio to make purchases
1 vote -
Please let the BNO055 go Grove!
The BNO055 is a neat orientation sensor which reduces the hassle of 3D orientation programming a lot. I would love to see this sensor (which has an I2C output) paired up with a Grove connector!
7 votes -
Add order status in the order information.
Add the order status in the order detail information.
2 votes -
Shipping Information
Can't get shipping information
7 votes -
Industrial 4-20ma input and output GROVE modules
I wish to control and read Industrial Sensors and equipment using 4-20mA signals, using a neat Grove module.
Thanks.
2 votesDo you mean by “industrial sensors with Grove port”?
-
AC Voltage Measurement Sensor
I would like to be able to read the ac voltage upto 250 VAC and pass the value to an MCU such as an Arduino or Raspberry Pi. I suggest that an analog value between 0-1023 (5VDC) would be suitable.
I cannot see why this cannot be done as I see almost throw away measurement devices with an LCD screen. I just want the raw data without a screen.
An ability to also obtain amps and hertz either as a consolidated sensor or 3 separate sensors would be even better.
Thank you5 votes -
Adapter Boards
I would like to be able to put smaller pitch components onto a regular breadboard.
Currently I have a number of leads from a mother board that fit very small pitch connectors. I need to be able to breakout these headers to fit onto a regular breadboard.
I cannot even find prototype boards with other than 2.54 pitch holes, let alone a dual size board.
Adapter boards that allow a dual row small pitch header to be fitted that breakout to standard size would be great. Currently I have 16 pin, 8 pin and 6 pin dual row headers that…1 vote -
Correct your weeb page
http://www.seeedstudio.com/service/index.php?r=pcb&ref=banner_fusion_fusion201631
in this page it says 4.9$ for 10 pcs but when you click it it changes to $9.9
why it is different ?3 votes -
Data storage expansion for the RePhone.
It would be great to be able to expand the RePhone memory, either to have a module that increases the flash memory or a module for a SD card reader, anything that could increase the only 5mb storage that is available in the RePhone.
3 votes -
Accumulate Order
Your recent Flash Sales are great, but if I could pay for then combine my orders from multiple flash sales then I can save on postage costs and pay postage separately at the end. But it does mean you will need to set aside each order until the end or give buyer option.
1 vote -
Linkit Assist 2502 Wiki and Projects
Complete support and Wiki page for Linkit Assist 2502. It says it works with xadow but nothing is clear in the manual provided by mediatek and not even a single project image or video on the internet. Makes me skeptical whether to buy the kit or not because after buying it, I won't be able to know how to handle it.
1 vote -
21 votes
-
6-layer boards, 35\my\ on inner layers, metal-filled vias, "0.1500".
Indeed 4 points...
1) 6-layer boards
On my WishList I have 6-layer boards.
2)
Another point is 35\my\ of coippeer on inner layers
3)
The option to have vias or holes in SMD pads metal-filled (as some PCB manufacturers offer). Or the simplified "poor-mans method" to add a third solder-mask which just adds "lids" over the holes on top or bottom side; controlled with an additional "Via Key" layer.A "SMD pad with a hole" is a pad defined as a through-hole with the top-layer shape the shape of "the same" SMD pad, a circular shape in other layers.
4)
How…7 votes -
Make an HC11/12 development kit available.
433MHz comms are used by many devices and the 433MHz chip on the HC12 has a lot of capabilities. If an IDE were available then the HC12 board could be adapted by developers for purposes beyond the standard FU1/2/3 usage.
2 votes -
I want to pay extra for options
Dear, I want to pay USD 10 for my PCB project extra because of panel. How can I do this?
1 vote -
A new DSO Quad
New hardware ! 4 real analog channels, 10-12 bit samples, at least 100MS/sec (per channel !). Improved "front end" and significantly more waveform memory (micro SD). Try to maintain the price point.
1 vote -
Official Raspberry Pi Touchscreen - Power bridge
Official touchscreen has a long jumper cable for power.
This can be much nicer with two small PCBs.
There may also be a micro-usb connector for the power supply.1 vote -
WS2812B breakout board does not say how many are in the package
http://www.seeedstudio.com/depot/WS2812B-LED-Breakout-Board-p-2010.html
I can't figure out how many I'm going to get, because it doesn't say. The picture shows five, but one commenter received only one. Please add a number to the description saying how many WS2812B breakout boards I will receive if I order one unit.
2 votes
- Don't see your idea?