My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
554 results found
-
Put an information sheet into arduino shield products sold at Radio Shack.
You need to put instructions into the boxes of products that go to Radios Shack. I spent over 2 frustrating hours combing both sites for information. And still I do not know the pins that I need to toggle to turn on relays from my "Seeed Studio Relay Shield." Is it too much to ask for a pinout and sample code? Or at the very least a LINK TO A WEB PAGE WITH THAT INFORMATION??????
3 votes -
Support Target3001 files
Support Target3001 Files
3 votes -
3 votes
-
You put the order tracking system in order. just try to track RF317795303SG on Singapore using the existing system.
Go back to the old system. It worked.
3 votes -
Allow me to pay
I selected, I addressed, I wanted to pay, I chose VISA, error - choose payment method.
I'd like to give you money.
But, well fix it enough that I know what you want, or don;t take it, up to you.3 votes -
Wireless charging for Super Capacitor
A wireless charger that can charge a Super Capacitor [SC]. It would have an adjustable maximum voltage of 2.0 to 2.5 volts, and be able to dump large amounts of current [5A or more -- much more] into an extremely low impedance load [i.e. a current source with an upper voltage limit]. Also, it should be able to dump current into the SC at full bore all the way up to the maximum voltage. A typical SC has a maximum voltage of 2.7 volts, but should not be charged higher than around 2.2 to 2.5 volts [the higher the voltage…
3 votes -
Seeeduino 1284P
I would like a Seeeduino 1284P. I really like Seeed's configuration of
the mega better than arduino's, however I feel that the 1284p has
the right amount of I/O and storage with more RAM than the 2560.3 votes -
HS code
you should post an option of "the number of harmonized system code or the number of tarif code" for international purchases.
3 votes -
Pass the shipping consignment number to the tracking site.
Pass the shipping consignment number to the tracking site.
The order tracking popup is a terrible way to incorporate order tracking: use a proper page or a panel on the base page. I can't select text from the layered panel on my tablet browser.
The track order link doesn't seem to pass the consignment number, which would make sense.
3 votes -
USB or Grove barcode readers
Need some USB or Grove barcode readers that can be used with BeagleBoneGreen.
3 votes -
3 votes
-
Add signup link to login page
Simple, and pretty typical.
3 votes -
We need a MagnetoPot Potentiometer in Grove ...
http://www.spectrasymbol.com/potentiometer/magnetopots
Build us a MagnetoPot Potentiometer leaf to plug into Grove. This will allow the monitoring and response to motion using a solid state contactless sensor. These particular Pots monitor over a longer range of motion so will be highly flexible and useful in there applications for many projects and Grove user applications.3 votes -
Data storage expansion for the RePhone.
It would be great to be able to expand the RePhone memory, either to have a module that increases the flash memory or a module for a SD card reader, anything that could increase the only 5mb storage that is available in the RePhone.
3 votes -
Correct your weeb page
http://www.seeedstudio.com/service/index.php?r=pcb&ref=banner_fusion_fusion201631
in this page it says 4.9$ for 10 pcs but when you click it it changes to $9.9
why it is different ?3 votes -
allow me to see prices in Canadian Dollars
I want to be able to change from USD to CAD so that I can see how much I'm paying before I order.
3 votes -
Your Verification button says its case sensitive but codes only show upper case. In short it dont work!
Fix your Verification box so that it shows both upper and lower case letters properly. I do not have time to be dicking around trying to figgure this out.
3 votes -
Please make a HomePlug shield!
WiFi is fine but HomePlug is better! So please make a shield for the BeagleBones.
3 votes -
Please add the 5 GHz to your BeagleBone Green! Or launch the BeagleBone Orange with the 5 GHz only WLAN. Should be rather easy to do...
Without doing my homework I think that the 5 GHz WLAN could be done just by WLAN controller and crystal changes and even the board could be essentially the same.
3 votes -
No pagination would be great, instead use "infinite" scroll
I really don't like browsing in paginated overview pages
3 votes
- Don't see your idea?