Anonymous
My feedback
-
9 votes
An error occurred while saving the comment -
5 votes
An error occurred while saving the comment Anonymous commented
The implementation of this API is likely to stream audio to remote servers to perform speech recognition. As such this API is not intended to be used for continuous recognition, which would consume a significant amount of battery and bandwidth. https://litebluelogin.us/
-
1 vote
An error occurred while saving the comment Anonymous commented
Aluminum can be brushed and does not require a finish although anodizing or powder coating is recommended. Plain steel can be brushed but requires a finish such as powder coating to prevent rust. Stainless steel can be brushed and does not require a finish. Plastic does not require a finish. https://liteblue.me
An optoisolator (also known as optical coupler, optocoupler and opto-isolator) is a semiconductor device that uses a short optical transmission path to transfer an electrical signal between circuits or elements of a circuit, while keeping them electrically isolated from each other.https://telldunkin.us