My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
- or
No existing idea results
- ~ No ideas found ~
554 results found
-
No hotline provided in order to call
Please provide a customer hotline.
1 vote -
How do I know if I am ordering a 15001K or a 15002K? The order form shows no choices.
There are two models how do I get to pick one
1 vote -
attach a file to question
Allow me to attach a file to message
2 votes -
Mix and Match PCB
Mix and Match PCB, get 10 boards for the current rate but be able to make it a combination of up to three layouts.
1 vote -
Manual of DSO nano V3
Page 3
▌Temperature:
Working condition:+0℃ to +500℃+500℃ or +50℃ ?
1 vote -
zero support from CHina
why don't you try and answer your customers questions instead of ignoring us?
1 vote -
Cart sharing capability. I would like to send the cart to my supervisor by email.
Cart sharing capability. I would like to send the cart to my supervisor by email.
3 votes -
MY SON
PLEASE FIND MY SON
1 vote -
1 vote
-
1 vote
-
?
customer support, when I ask a question, I want an answer, TODAY
1 vote -
3 votes
-
"What are the Fusion PCBA status?" is missing "BOM Awating packing" - what is that?
Adding to "What are the Fusion PCBA status?" the missing "BOM Awating packing" - what is that?
1 vote -
Deliver what you promiise
Try manufacturing PCB's instead of just taking money on the pretence that you do
1 vote -
How about including the file name information on the ORDERED screen so that customers can see what they have actually placed an order for.
How about including the file name information on the ORDERED screen so that customers can see what they have actually placed an order for.
I currently have a multiple order in place, with more boards required.
My problem is that I can not see which boards "names" are currently in the queue and I therefore have to wait until all of the boards have arrived here "at home base" tobefore I can place my next order.
Thanks.1 vote -
better service
When you show under order history to Reupload a file also list the problem with the existing file so it can be fixed quickly.
1 vote -
Ehter
Payment with Ether.
1 vote -
Grove board for Mics 4514
Hi,
Alternatively to the Mics 2714 (recently suggested) you could produce one for the Mics 4514 which combines both nitrogen dioxide and carbon monoxide.
There is already an open HW specification with Arduino code here:
https://github.com/ShawnHymel/MICS-4514_CO_and_NOx_Sensor_BreakoutThanks!
1 vote -
Grove sensor for MiCS 2714 (nitrogen dioxide)
Hi,
I would really love to see the Mics 2714 sold in a nice board with a GROVE connector. The Mics 2714 measures probably the most important pollutant, Nitrogen Dioxide. The datasheet comes with an example interface circuit (few resistors) for a 5V microcontroller.
Thanks!
1 vote -
When 2g is turned off my SMS GSM modem wont work. I will need along with 1,000's of others a simple 3g - 4g modem to interface to alarm syst
When 2g is turned off my SMS GSM modem wont work. I will need along with 1,000's of others a simple 3g - 4g modem to interface to alarm syst
1 vote
- Don't see your idea?