My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
Gerber drill generator needs updating
The CAM job needs to be updated for eagle 7.0+ to use Excellon_24 instead. Otherwise, the dimensions of the drill file doesn't work.
1 vote -
Motor Driver Board V1.0
This board needs to be redesigned as it cuts out the RPi when the motors activate. There does not seem to be a solution
1 vote -
Your online BOM List can not be filled. Please fix it.
Bom list can not be filled online. Online list does't show.
4 votes -
Mentor Gerber Format
Complete procedure to get the PCB, Mentor Graphics is the software
1 vote -
wonder if seeed has anything that could send an sms when the diaper is wet ;)
wonder if seeed has anything that could send an sms when the diaper is wet ;)
1 vote -
e-ink or oled starter kit
arduino to make mimi bt display unit and connect to mobile
1 vote -
Fix your site
fix your site so that you are giving the correct tracking numbers, not fake or tracking number for a previous shipment. I recently purchased a product in october. status is tracable but tracking number is for a shipment in august?!?!? how is this even possible?
1 vote -
Pass the shipping consignment number to the tracking site.
Pass the shipping consignment number to the tracking site.
The order tracking popup is a terrible way to incorporate order tracking: use a proper page or a panel on the base page. I can't select text from the layered panel on my tablet browser.
The track order link doesn't seem to pass the consignment number, which would make sense.
3 votes -
payment method
Better, more reliable payment method.
3 votes -
sell thermoplastic extruders like the WEE KIT from FILABOT.COM for recycling prints from 3D Printers
with the proliferation of thermoplastics like water bottles and "prints" from 3D Printers, why not sell a kit that would allow individuals, schools, and companies that have lots of waste prints to make their own filament material like the KIT EXTRUDER from http://www.filabot.com ?
1 vote -
Free talk at FSOSS "fRephone" http://fsoss.senecac.on.ca/2015/schedule
I could talk about Rephone at Seneca in Toronto next week. Ask dumb questions and become undumbina-ted
1 vote -
1 vote
-
2.8" TFT-Touch display uses flip and rotate coordinates and callback functions for touch
I'd like to draw your attention to the library extensions I wrote for the 2.8" TFT-Touch display with resistive touchscreen.
Please visit:
http://86.91.251.42/JanBeeProjects/TFT_Touch2p8inch/TFT_Touch2p8.htmThese extensions to the TFTv2 library allow flipping and rotating the coordinate system and implement a simple to use system for bookkeeping of touch-sensitive areas, using call-back functions.
You may publish these files and the demo projects as you like.
Greetings, Jan Breemer, jan@breem.nl
1 vote -
Add a DTR Pin to the dual mode Bluetooth Device so that it can also flash the microcontroller over the air.
Currently the Bluetooth Modules with HM-13 are not providing the DTR Pin that is needed to reset the microcontroller while flashing a new firmware. It would be great if that functionality could be made available on one of the programmable Output Pins.
1 vote -
Adding LiPo battery support to BeagleBone Green
I suggest adding support for LiPo batteries to the BeagleBone Green.
As far as I can see in this post (http://www.element14.com/community/community/designcenter/single-board-computers/next-gen_beaglebone//blog/2013/08/10/bbb--rechargeable-on-board-battery-system) is just a matter of adding a LiPo battery connector and a resistor
1 vote -
More Cameras
More inexpensive-yet-good camera modules composed of OVM cameras with flex cables.
1 vote -
Create a board like the BBG but without any connectors
There are so few companies that are making modules like the BBB/BBG without the ethernet & USB connectors. This is an embedded market product so lets make it that way. I want to plug the module into my circuit board and put the connectors where I need them to be.
5 votes -
Make the DMX512 PCB board finish flush with the edge of the three pin socket
When trying to mount the DMX512 board I had to cut off 3mm of PCB to allow the socket to sit flush with the mounting hole.
Please finish the PCB flush and put a mount hole on the side instead. Note, I'd put it on the side of the high screw hole to stop socket twisting on insertion of lead. Photos attached
4 votes -
Fix you Stalker V3 Defect
fix your P5 defect on the Stalker V3
1 vote -
easy way to personnalize rephone paper craft box
Send me your box shape for rephone as i could include it into my site http://www.visualkit.com (or in a separate one), and provide an easy way to personnalize it. Or perhaps you prefere do your own ...
1 vote
- Don't see your idea?