BitCoin payment option would be great!

39 comments
-
Diana Adams commented
Thanks for suggestions. I will try to use bitcoin for payment. I've never done this before. I would like to share with you an interesting and up-to-date mobile development company blog https://mlsdev.com/ I always read it and advise you too.
-
Red Arrow commented
I agree it would be great. I am as a trader possess some bitcoins and I would like to try to spend them. By the way, if you are also a trader, you should have a look at the best crypto signals! Us traders should support each other!
-
mark commented
Please do not add bitcoint payment for the sake of the environment. One single transaction currently wastes the electricity consumption of 24 days of an average household. Please read up on the evil "proof of work" algorithm it uses.
-
Anonymous commented
Yes, you have the right option. It will be good for all to use bitcoin as paypal and payoneer have many other issues, https://gta5files.com/
-
robinmalhotra commented
Please utilize this sticky thread for all general Bitcoin discussions! If you see posts on the front page or new which are better suited for this daily discussion thread, please help out by directing the OP to this thread instead. Thank you!
If you don't get an answer to your question, you can try phrasing it differently or commenting again tomorrow.
https://appsync.biz/speed-test/ https://appsync.biz/scrabble-word-finder/ https://appsync.biz/solitaire/
-
Andrew commented
yes... This method of payment is really good and secure rather than offering cash or by paying through credit/debit cards... Bitcoins is a crypto-currency. So, It can be used in this payment method also... I just want to clarify here... Is there any threat of frauds calls and losing bitcoin?? https://mobdro.ooo
-
Barry Flash commented
We are developing an ICO where the investor finances the IoT device (made by seeed Studio) and in exchange gets a % of the revenue that the IoT device produces under smart contract in its life cycle so in order to built credibility into the ICO token the ether will be released directly to the IoT manufacturer under Smart Contract once the first batch is registered into the https://radrdetector.com/best-radar-detector-reviews/ Ethereum blockchain as a Proof of Existence
-
greyworm commented
We are developing an ICO where the investor finances the IoT device (made by seeed Studio) and in exchange gets a % of the revenue that the IoT device produces under smart contract in its life cycle so in order to built https://freemoviesite.me/sportsarefree-xyz-alternatives/ credibility into the ICO token the ether will be released directly to the IoT manufacturer under Smart Contract once the first batch is registered into the Ethereum blockchain as a Proof of Existence
-
Anonymous commented
I will go a step further and it is considering no only in acepting ether and bitcoin as an altenative payment but also acept participate in ICO as a Beneficiary (Independent (pre-paid) Dynamic Beneficiaries
We are developing an ICO where the investor finances the IoT device (made by seeed Studio) and in exchange gets a % of the revenue that the IoT device produces under smart contract in its life cycle so in order to built credibility into the ICO token the ether will be released directly to the IoT manufacturer under Smart Contract once the first batch is registered into the Ethereum blockchain as a Proof of Existence
-
Anonymous commented
There are a number of third-party services which handle Bitcoin payment processing into regular currencies, that might make implementing this easier and safer for you.
While many people won't use it, I don't really see any valid reason NOT to add it, and accepting it while other sites don't gives you an advantage attracting customers.
-
Bob commented
If paypal is complicated for you, then you must be a fifth-grader.
Forget bitcoin, its for money laundering only. -
Chris S. commented
Please add Bitcoin. I'd use it regularly just like I do with Fasttech.com. I often get paid in BTC so being able to spend it without dealing with paypal (which is complicated for me) would be awesome. You can integrate it using Bitpay as many do (including Fasttech).
-
Anonymous commented
I would definetely buy in bitcoins if this site supports it.
-
Simon Peacock commented
Forget Bitcoin. Although bitcoin is a cool idea, without government acceptance it lends itself to money laundering and criminal activity, transactions will eventually be blocked (somehow) or bitcoins will be traced back to a criminal event in which case the bitcoin would be treated as stolen property and forfeited.
-
Gitle M commented
Bitcoin support would be great. If you as the first low cost PCBA supplier accept bitcoin, you would gain me as a loyal customer.
The commenter below me is missing the point, Paypal may work well for him, but it doesn't for everybody, that's just a fact. There are several countries where paypal is simply unavailable, and yet others may choose to avoid it for various reasons. By accepting bitcoin you would increase the amount of potential customers, and its core userbase perfectly aligns with your target audience: engineers and other tech savvy people.
-
Graham commented
Forget bitcoin. There's nothing wrong with PayPal; I've used it since 2002 with zero problems, as have millions of other people. Anyone who has an issue with PayPal is probably trying to cheat the seller. All of PayPal's problems are connected with suspicious use of funds, admittedly not all of them justified, but buying printed circuits boards is hard to classify as suspicious.
-
Anonymous commented
Bitcoin sucks.
-
Oliver commented
It would be wiser to find a payment service that automatic converts not only bitcoin but another altcoins as well. More payment options = more costumers. ;)
-
Anonymous commented
Hi, bitcoin as payment method really would be great since it's the only reasonable method for us in order to buy at seeed bazar or fusion. Paypal is a no-go since it has such a rotten stance. Alipay isn't an option at all for us living in europe. So, please introduce bitcoin.