My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
147 results found
-
Plase fix the shopping cart!
In an earlier step I added an item to the shopping cart which I now don't need anymore.
But there is no function to remove an item: no "remove" link and button "-" only reduces count down to "1" but not to "0".
Please fix this asap, as I cannot order anything by now without also ordering the superfluous item.
Second, you suggest to go to shopping cart and use the link "estimate shipping costs" if you want to know how much shipping will cost before checkout ... Nice! But there is no such link!
3 votes -
Shipping Information
Can't get shipping information
7 votes -
21 votes
-
iran
would you please describe it in a clear way that how can I purchase some ordinary components from Iran?
10 votes -
Add back facebook login
I use to login with facebook and order several orders. But I cannot do it with new website
6 votes -
Offer PCB in Raspberry Pi HAT size ( 65mm x 56mm )
Offer PCB size 65x56 for Raspberry Pi Hat.
ATM I have to order 100x100 Board to get 65x56 Raspi Hat.10 votes -
GSM for Pebble
Can we connect the GSM module to Pebble? because I want to leave my phone :), I wait for your comments.
3 votes -
Stackup information PCBs
Information about the stackup for a four-layer PCB.
I would be nice to have a stackup for every PCB thickness seeedstudio provides. This makes impedance based routing possible.124 votes -
Need to know if there is free shipping to Beijing
I urgently need to know if there is any free shipping to Beijing area.
Also Transit time and if there is no free shipping then cost to shipping Beijing.
4 votes -
Please let the BNO055 go Grove!
The BNO055 is a neat orientation sensor which reduces the hassle of 3D orientation programming a lot. I would love to see this sensor (which has an I2C output) paired up with a Grove connector!
7 votes -
Industrial 4-20ma input and output GROVE modules
I wish to control and read Industrial Sensors and equipment using 4-20mA signals, using a neat Grove module.
Thanks.
2 votesDo you mean by “industrial sensors with Grove port”?
-
Kicad lib for OPL
Create an OPL lib for Kicad
13 votes -
AC Voltage Measurement Sensor
I would like to be able to read the ac voltage upto 250 VAC and pass the value to an MCU such as an Arduino or Raspberry Pi. I suggest that an analog value between 0-1023 (5VDC) would be suitable.
I cannot see why this cannot be done as I see almost throw away measurement devices with an LCD screen. I just want the raw data without a screen.
An ability to also obtain amps and hertz either as a consolidated sensor or 3 separate sensors would be even better.
Thank you5 votes -
Add order status in the order information.
Add the order status in the order detail information.
2 votes -
6-layer boards, 35\my\ on inner layers, metal-filled vias, "0.1500".
Indeed 4 points...
1) 6-layer boards
On my WishList I have 6-layer boards.
2)
Another point is 35\my\ of coippeer on inner layers
3)
The option to have vias or holes in SMD pads metal-filled (as some PCB manufacturers offer). Or the simplified "poor-mans method" to add a third solder-mask which just adds "lids" over the holes on top or bottom side; controlled with an additional "Via Key" layer.A "SMD pad with a hole" is a pad defined as a through-hole with the top-layer shape the shape of "the same" SMD pad, a circular shape in other layers.
4)
How…7 votes -
Update the WIKI
New products or new versions of products, Grove Temp sensor V1.2, could not find it. Many bad links. Kit products with new version of hardware but wiki goes to old version of the product. Grove Starter Kit for Arduino V3 has some in it. New products or versions of products in the store going to old versions on wiki. I think the store and the wiki could use a good going over and clean up.
7 votes -
wired/wireless Grove-controlled 220V outlets
A simple, wired outlet is something I find myself making all the time (left side of photo), but I'd rather buy something smaller/safer/nicer than keep making them :)
The [more expensive] wireless product can have the same functionality of a "normal" rf (or ir) controlled outlet, but the remote control would also have a grove socket. If it's necessary to have 2 buttons/pins in order to control such a device (like the a/b buttons in the photo), you can use both yellow and white lines (unorthodox for non-I2C grove modules, but I don't see any reason why not).
10 votes -
Create a board like the BBG but without any connectors
There are so few companies that are making modules like the BBB/BBG without the ethernet & USB connectors. This is an embedded market product so lets make it that way. I want to plug the module into my circuit board and put the connectors where I need them to be.
5 votes -
wonder if seeed has anything that could send an sms when the diaper is wet ;)
wonder if seeed has anything that could send an sms when the diaper is wet ;)
1 vote -
3G version of LoNet 808 - Mini GSM/GPRS + GPS Breakout, SKU: 113990107
Simcom based. SIM5320E or another 3G & GPS Simcom chip.
1 vote
- Don't see your idea?