Jeff Brown

My feedback

1 result found

  1. 10 votes
    How important is this to you?
    An error occurred while saving the comment
    Jeff Brown commented  · 

    Spraying Equipment

    The Dualsteer® is a patented double steering system that combines the central articulation of the frame with the steering of the front wheels: this allows to realize a real steering angle equal to 70°, with the greater percentage of steering to the wheels of the front axle for ensure greater directionality.

    From the operational point of view the driver only needs to operate the steering wheel because the control of the engagement proportionality of the two devices, which act simultaneously, is guaranteed by a hydraulic circuit and by a specific system of mechanical connection of synchronization. The hydraulic circuit acts both on the steering cylinders of the central articulation and on the steering cylinders of the front wheels while the connection system guarantees the synchrony and the progressiveness of the steering.

    The additional hydraulic cylinder on the central steering increases both the power steering with high accuracy at very low speeds also in presence of high load on the axles, both the direction and stability on road transfer at high speeds.

    The Dualsteer® system therefore combining safety and stability of the steering wheel (RS) version with the steering performance and manoeuvrability of the version with central articulation (AR).

    https://tractors.ae/sprayingequipments.php

Feedback and Knowledge Base