My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
- or
No existing idea results
- ~ No ideas found ~
554 results found
-
Exclude discontinued items from listings.
It's getting where there are more discontinued items than new ones. It would be nice if the discontinued items were only visible if you visited the item directly. (Preventing broken links). Otherwise exclude them from the default view.
3 votes -
Your mobile site stinks
Include the option to choose desktop site view on all devices.
3 votes -
LoRa GW, SKU 110060623, would sell well at $200
There are a number of "complete LoRaWan gateway" in the $240 to $300 range... Making this incomplete KIT expensive...
1 vote -
Extension Cable for Grove
I wish there was a male-female Grove cable with, let's say, 100 cm as a extesion cable. Alternatively a tiny male-male PCB could act as an "extension adapter".
4 votes -
make it clear what order statuses are on web
on website under order keep status of the order updated like:
- validating order
- manufacturing started:
- stencil done (10%)
- routing done (30%)
- vias done (40%)
- solder mask done (70%)
- packing done (100%)
- shipped out2 votes -
Split shipping packages
Is any way possible to add an option to split the number of packages? I need 400 boards in 4 packages
1 vote -
UPS board for generic SBC
There are few boards with native lithium battery support but it would be nice to add UPS like function to any 5V powered board, be it ARM or Atmel. AXP209 is integrated on some boards and I believe it would be very interesting to have it on a breakout board similar with a solar charge controller. The simplest configuration would have only 6 pins (5V--In&GND / Batt+&Batt- / 5V-Out&GND). Some extra feature would make it even better: an EN pin that would cut-off both battery and Vin input. An AO pin to measure the battery voltage, a DO to send a battery low signal (whenever the analog inputs are unavailable). Or even better, have an I2C interface that would send various readings to the SBC (input current and voltage, output current and voltage, battery voltage, IC temperature and any other geeky stuff that you can think of). Also some exposed PCB solder points should be available to configure the battery protection specs. Most of basic battery protection circuits cuts down the power when the battery voltage reaches 2.5V but this is way too low compared to the vendor's recommended value. Having the option to set the overdischarge voltage protection at 3V would be great in order to protect the batteries.
Adafruit's Powerboost 1000C does the basic functions but it's quite expensive and fairly large. A smaller (PCB and breadboard friendly to be used with flat LiPo as well as 18650 PCB mounted batts) and cheaper alternative would be great. And a deluxe version with all those extra features would be even greater.There are few boards with native lithium battery support but it would be nice to add UPS like function to any 5V powered board, be it ARM or Atmel. AXP209 is integrated on some boards and I believe it would be very interesting to have it on a breakout board similar with a solar charge controller. The simplest configuration would have only 6 pins (5V--In&GND / Batt+&Batt- / 5V-Out&GND). Some extra feature would make it even better: an EN pin that would cut-off both battery and Vin input. An AO pin to measure the battery voltage, a DO to send…
3 votes -
include the tubing for the smart plant care kit fir arduino. Or at the very least include the specifications for the vinyl tubing.
I had to order vinyl tubing because it was not included in the kit. There are no specifications for the tubing so I ordered something that looked like it would work. As it turns out the vinyl tubing that I ordered was incorrect so i had to order another size of vinyl tubing. After ordering 2 packages of vinyl tubing through Amazon and waiting over 2 weeks i finally got tubing that fit (on one part of the kit but not the other). I am very frustrated because this could be easily avoided with better instructions or the inclusion of the necessary tubing. I have now had this kit for almost a month and it is still not working.
I had to order vinyl tubing because it was not included in the kit. There are no specifications for the tubing so I ordered something that looked like it would work. As it turns out the vinyl tubing that I ordered was incorrect so i had to order another size of vinyl tubing. After ordering 2 packages of vinyl tubing through Amazon and waiting over 2 weeks i finally got tubing that fit (on one part of the kit but not the other). I am very frustrated because this could be easily avoided with better instructions or the inclusion of…
1 vote -
A better support from SeeedStudio
Pretty simple a better support.
It is a must.
7 votes -
eC compitable stencil and PCB, and visual check tool like Eurocircuits have
Can you add the option (like on the Eurocircuits website) to make PCB and stencil compatible with the eC standard?
Eurocircuits is a European PCB manufacturer, they sell a common used stencil machine the eC-stencil-mate:
http://www.eurocircuits.com/ec-equipment-ec-stencil-mate/
The eC standard can be found here:
http://www.eurocircuits.com/ec-registration-system/
Here you can find the option:
http://be.eurocircuits.com/shop/orders/configurator.aspx
eC-registration compatible PCBIt is also recommended to make a visual check tool, such as Eurocircuits have.
5 votes -
24-bit 192 kHz 120 dB S/N audio DAC
A reference quality 24-bit, 192 kHz, >120 dB S/N ratio audio DAC cape for all Beagle Bones.
1 vote -
CISECO SRF Module (used on
I would like to by about 20 pc. of the CISECO SRF Module (used on CISECO SRF Shield). Will it get available again ?
2 votes -
Smaller stensels
My PCBs are all very small and I hand screen and place components. Any chance of getting a screen that is 10 mm or so bigger all around than the PCB.
No need to pay high shipping costs for a screen that I have to cut up to use.
3 votes -
"Seeed Fusion’s Awarded questionnaire" Letter
"Seeed Fusion’s Awarded questionnaire" e-mail is broken - link inside it leads nowhere, its just "fusion-questionnaire.html?key=*****" without complete URL
2 votes -
A relay shield with Capacitor on each that can be adjusted. as well as a potentiometer
A relay shield with Capacitor on each that can be adjusted. as well as a pot on each.also an ferrouse metal sleeve where you tie in the leads to keep the power from to stablize voltage. We also need a singing tesla coil wireless power transfer shield. hell even if its just for the crazy texan
1 vote -
that you PLEASE fix the wiki for GPRS Shield V2.0
that you PLEASE fix the wiki page for GPRS Shield V2.0.
It comes up totally blank.
http://wiki.seeedstudio.com/wiki/GPRS_Shield_V2.01 vote -
Add button to change order status in order history
In my order history I have several order marked as "Traceable" but I receive the order.
Add a user button to change the status to "Finisced"
1 vote -
1 vote
-
20x4 LCD Module for raspberry pi zero
just like this seeedstudio product
https://www.seeedstudio.com/Raspberry-Pi-RGB1602-LCD-Module-p-2803.html
but for 20x4 LCD Module for raspberry pi zero. all electronics and buttons should be on the back of shield, so it looks clean.1 vote -
You're web page isn't working well with me, get it right!
I, for instance, want to see all Grove products in Bazar.
Make it easier to browse your web.1 vote
- Don't see your idea?