My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
Kicad lib for OPL
Create an OPL lib for Kicad
13 votes -
Seeeduino 1284P
I would like a Seeeduino 1284P. I really like Seeed's configuration of
the mega better than arduino's, however I feel that the 1284p has
the right amount of I/O and storage with more RAM than the 2560.3 votes -
Single board computer with embedded 3g modem
I just saw the RePhone and the Linkit One, but these are powered by microcontrollers, why not develop a single board computer like the Beaglebone green or Raspberry Pi but with an embedded 3G modem and LiPo battery support
2 votes -
RGB laser diode
Create an RGB laser out of Laser Diodes
1 vote -
Fusion/Seed higher prices now? Why? China's economy is in slump!
Why Fusion/Seeed Studio is squeezing more money of the customers? Prices are higher, while China's economy has crashed!!!!!!
1 vote -
Impedance Calculation Utility
A calculation tool to let customers know the impedance of their PCB traces.
Here is an example:
http://www.hughescircuits.com/index.php/en/support/impedance-calculatorThe customer would only need to enter their PCB trace width, because all the other parameters can be determined automatically from the PCB specifications that the customer has selected.
10 votes -
HS code
you should post an option of "the number of harmonized system code or the number of tarif code" for international purchases.
3 votes -
Price for printing 10x15cm size Fusion PCBs
Reduce the price of printing 15x10cm size fusion PCBs
1 vote -
I would to see a GPS Bee with a backup battery. So far every start is a cold start.
I would love to see a GPS Bee with a backup battery. So far every start is a cold start.
1 vote -
A decent customer service.
A decent customer service.
2 votes -
Make available source code for the Skeleton Bot
- 4WD Hercules Mobile Robotic Platform. Would be very handy currently all wheels travel the same direction? Please upload the code you used to create the car in the video. I dont understand how to control the wheels.
1 vote -
Build a Grove MQ136 Sensor
I would like Seeed to build a MQ136 sensor for H2S as a Grove unit (stem). I prefer Grove to Sain ... http://www.sainsmart.com/sainsmart-mq136-gas-sensor-hydrogen-for-arduino-mega2560-uno-r3-raspberry-pi.html
Thanks
2 votes -
7 votes
-
due to this limitation "Minimum inner trace width(for 4 layers) 0.204 8" I can't use QFP with 0.5mm like STM32f407VET6
use same DRU fort 2 layer and 4 layer ? At least for TOP and Botton layer in order to use standart packages.
1 vote -
Wireless charging for Super Capacitor
A wireless charger that can charge a Super Capacitor [SC]. It would have an adjustable maximum voltage of 2.0 to 2.5 volts, and be able to dump large amounts of current [5A or more -- much more] into an extremely low impedance load [i.e. a current source with an upper voltage limit]. Also, it should be able to dump current into the SC at full bore all the way up to the maximum voltage. A typical SC has a maximum voltage of 2.7 volts, but should not be charged higher than around 2.2 to 2.5 volts [the higher the voltage…
3 votes -
3G version of LoNet 808 - Mini GSM/GPRS + GPS Breakout, SKU: 113990107
Simcom based. SIM5320E or another 3G & GPS Simcom chip.
1 vote -
Grove Lib for Linkit assist 2502 SDK (which also works with Linkit one)
create a grove lib that hooks into the linkit assist 2502 sdk. This lib would work with linkit one as well which would enable more advanced development with the linkit one
1 vote -
Stackup information PCBs
Information about the stackup for a four-layer PCB.
I would be nice to have a stackup for every PCB thickness seeedstudio provides. This makes impedance based routing possible.123 votes -
Fusion PCB Specification -- Provide separation dimensions between layers.
For computing strip-line impedance it is important to know the distance between conducting layers and the dielectric constant of the insulator material. If averages are provided please also provide variance
21 votes -
Support TI C2000 for Crazyflie
You could allow C2000 launchpad plug into actuators and sensors to control Crazyflie
1 vote
- Don't see your idea?