My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
- or
554 results found
-
Fix you Stalker V3 Defect
fix your P5 defect on the Stalker V3
1 vote -
easy way to personnalize rephone paper craft box
Send me your box shape for rephone as i could include it into my site http://www.visualkit.com (or in a separate one), and provide an easy way to personnalize it. Or perhaps you prefere do your own ...
1 vote -
Seeeduino 1284P
I would like a Seeeduino 1284P. I really like Seeed's configuration of
the mega better than arduino's, however I feel that the 1284p has
the right amount of I/O and storage with more RAM than the 2560.3 votes -
A decent customer service.
A decent customer service.
2 votes -
RGB laser diode
Create an RGB laser out of Laser Diodes
1 vote -
Build a Grove MQ136 Sensor
I would like Seeed to build a MQ136 sensor for H2S as a Grove unit (stem). I prefer Grove to Sain ... http://www.sainsmart.com/sainsmart-mq136-gas-sensor-hydrogen-for-arduino-mega2560-uno-r3-raspberry-pi.html
Thanks
2 votes -
Price for printing 10x15cm size Fusion PCBs
Reduce the price of printing 15x10cm size fusion PCBs
1 vote -
due to this limitation "Minimum inner trace width(for 4 layers) 0.204 8" I can't use QFP with 0.5mm like STM32f407VET6
use same DRU fort 2 layer and 4 layer ? At least for TOP and Botton layer in order to use standart packages.
1 vote -
Wireless charging for Super Capacitor
A wireless charger that can charge a Super Capacitor [SC]. It would have an adjustable maximum voltage of 2.0 to 2.5 volts, and be able to dump large amounts of current [5A or more -- much more] into an extremely low impedance load [i.e. a current source with an upper voltage limit]. Also, it should be able to dump current into the SC at full bore all the way up to the maximum voltage. A typical SC has a maximum voltage of 2.7 volts, but should not be charged higher than around 2.2 to 2.5 volts [the higher the voltage the lower the live expectancy so it's a tradeoff between performance and longevity]. Also, when a SC is fully discharged, it behaves like a direct short with a high current capacity path, so this wireless charger must be able to handle that without issue. The current sourced by this device doesn't need to be regulated and can even be a pulse of some sort [i.e. the raw, rectified output of the receiver] -- just as long as the voltage across the capacitor doesn't exceed the maximum voltage.
A wireless charger that can charge a Super Capacitor [SC]. It would have an adjustable maximum voltage of 2.0 to 2.5 volts, and be able to dump large amounts of current [5A or more -- much more] into an extremely low impedance load [i.e. a current source with an upper voltage limit]. Also, it should be able to dump current into the SC at full bore all the way up to the maximum voltage. A typical SC has a maximum voltage of 2.7 volts, but should not be charged higher than around 2.2 to 2.5 volts [the higher the voltage…
3 votes -
Grove Lib for Linkit assist 2502 SDK (which also works with Linkit one)
create a grove lib that hooks into the linkit assist 2502 sdk. This lib would work with linkit one as well which would enable more advanced development with the linkit one
1 vote -
Support TI C2000 for Crazyflie
You could allow C2000 launchpad plug into actuators and sensors to control Crazyflie
1 vote -
On the SARK-110 I would like to be able to offset the vertical axis and display the j reactive component rather than the Z impedance.
I have the SARK-110 and need to display the j component with vertical axis zero in the middle of the display. Thank you
1 vote -
Gerber Viewer doesn't show holes.
Worried that Seeed may not see the drill files in my Gerber.
6 votes -
Please Stock Netduino Wifi 3
Please Stock Netduino Wifi 3
1 vote -
Fusion PCB pricing
PCB should be priced by the total sq cm used & not by fixed length & width measurements. This would stop crazy price jumps. Build a board that is 5.54cm & you have to move up to 10cm size board pricing. This crazy & shouldn't be happening. Please price your boards fairer for the total area of the boards used & not for the area not used.
29 votes -
I would like to see more Grove Kits/Sensors offerings not associated with a platform. Or maybe a fill your own sensor "bag" of sensors!
I would like to see more Grove Kits/Sensors offerings not associated with a platform. Or maybe a fill your own sensor "bag" of sensors!
1 vote -
How about data on the Edsion Xadow product such as why things are not working? Also a test to tell you the thing is working? Flashing light.
Flasing lights don't anwer the question if the system is working? The OLED pretty much should have some indication there is power ? Nothing!! My only guess is the thing is bad from out of the box.
1 vote -
test leads with sharp tip
test leads with sharp tip, I suggest a better test tip for the measuring leads, made of a spring loaded test pin as the tip and a plastic pencil body; thus it stays firmly on even very thin pins even when the user looks to the measuring values or screen and the keeping force is not constant
1 vote -
Shipping needs major work
I had known it would take almost a week to send my order i would have ordered elsewhere.
6 votes -
MCPCB Service request
You add a Metal Core (MCPCB) option to your already excellent Fusion service.
1 vote
- Don't see your idea?