Ultrasonic Flowmeter
Flowmeter with ultrasonic transducer
There are some specialized chip, Max35104, Ams GP22/GP30 and Texas TDC7200
![](http://www.gravatar.com/avatar/8f0e8ed715ce2bc4450e2f37e653840a?size=40&default=https%3A%2F%2Fassets.uvcdn.com%2Fpkg%2Fadmin%2Ficons%2Fuser_70-6bcf9e08938533adb9bac95c3e487cb2a6d4a32f890ca6fdc82e3072e0ea0368.png)
-
jonah hill commented
Participate in Olive Garden Survey at ogtogosurvey and grab a fabulous opportunity to win a $1000 cash Prize.http://customerfeedbacks.site/www-ogtogosurvey-com/
-
Ava commented
There are a lot of site on the internet on this topic where you can found all of your answers easily and they also offer cost calculators for the reference i'm sharing a link with for more you have to google it. https://www.walmartonelogin.org/
-
Anonymous commented
Ultrasonic flowmeters use sound waves to determine the velocity of a fluid flowing in a pipe. At no flow conditions, the frequencies of an ultrasonic wave transmitted into a pipe and its reflections from the fluid are the same. When the fluid moves faster, the frequency shift increases linearly. http://www.krogerfeedback.com
-
DIODA2014 commented
Is it possible to measure air flows in the range of 500 ml/min?
HOw much is it cost?
Do you make international shipping to Argentina?
Thank you very much