A relay shield with Capacitor on each that can be adjusted. as well as a potentiometer
A relay shield with Capacitor on each that can be adjusted. as well as a pot on each.also an ferrouse metal sleeve where you tie in the leads to keep the power from to stablize voltage. We also need a singing tesla coil wireless power transfer shield. hell even if its just for the crazy texan
1
vote
![](http://www.gravatar.com/avatar/71116b64320e137595692cd7de15047b?size=40&default=https%3A%2F%2Fassets.uvcdn.com%2Fpkg%2Fadmin%2Ficons%2Fuser_70-6bcf9e08938533adb9bac95c3e487cb2a6d4a32f890ca6fdc82e3072e0ea0368.png)