跳到内容

My Seeed Idea

Share. Vote. Discuss. See.

Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!

To get help or support, download, or more information, please visit our wiki site.

554 找到的结果

  1. Create a board like the BBG but without any connectors

    There are so few companies that are making modules like the BBB/BBG without the ethernet & USB connectors. This is an embedded market product so lets make it that way. I want to plug the module into my circuit board and put the connectors where I need them to be.

    5
    0 条评论  ·  I wish  ·  管理员 →
    这对你有多重要?
  2. Rephone/Xadow Strap/Mesh kit

    Influenced by The RePhone project and the Pebble Time project. create a form factor custom strap/mesh kit which can house xadow parts (maybe Grove sensors) with a connection to RePhone/Wio Project. Each Xadow or Grove part is housed in a sturdy weather resistant container - to protect the electronics from damage/weather. Allowing the strap/mesh kit to connect with the Xadow flexible cables and Grove sensors so that it is attachable to clothing, walls (inside or out), poles, necks, vests etc.

    5
    这对你有多重要?
  3. AC Voltage Measurement Sensor

    I would like to be able to read the ac voltage upto 250 VAC and pass the value to an MCU such as an Arduino or Raspberry Pi. I suggest that an analog value between 0-1023 (5VDC) would be suitable.
    I cannot see why this cannot be done as I see almost throw away measurement devices with an LCD screen. I just want the raw data without a screen.
    An ability to also obtain amps and hertz either as a consolidated sensor or 3 separate sensors would be even better.
    Thank you

    5
    1 条评论  ·  I wish  ·  管理员 →
    这对你有多重要?
  4. Shipping

    Most companies have an option when ordering to find out what the shipping cost is.
    As you do not seem to have this option, I will order my Raspberry Pi from somewhere that has this option.

    5
    这对你有多重要?
  5. Speech Recognizer

    Customization for the initiation key word
    Customization for the response after command

    5
    这对你有多重要?
  6. 3D Model and Gerber Files

    Having gerber files or some data sheet to show the locations of the header placements for easier use. Having 3d model of the PCB with the connectors for easier use.

    5
    这对你有多重要?
  7. eC compitable stencil and PCB, and visual check tool like Eurocircuits have

    Can you add the option (like on the Eurocircuits website) to make PCB and stencil compatible with the eC standard?
    Eurocircuits is a European PCB manufacturer, they sell a common used stencil machine the eC-stencil-mate:
    http://www.eurocircuits.com/ec-equipment-ec-stencil-mate/
    The eC standard can be found here:
    http://www.eurocircuits.com/ec-registration-system/
    Here you can find the option:
    http://be.eurocircuits.com/shop/orders/configurator.aspx
    eC-registration compatible PCB

    It is also recommended to make a visual check tool, such as Eurocircuits have.

    5
    1 条评论  ·  I wish  ·  管理员 →
    这对你有多重要?
  8. USA Distributor or Cheaper Shipping

    This is why I can't use your products; I have $27 of Grove modules and the cost to ship them is more than twice that. Your shipping charges are way too high; or you need a distributor in the USA or cheaper shipping method

    5
    这对你有多重要?
  9. Why so long delay in production of PCB?

    Why is so long delay in PCB production?
    I have make order on 23.02.2018. and still today stay processing and I do not know when production will be start, then waiting on shippement. I am very disapointed with this. Now, after production wait another 20-30 days or even more that I become my orders, too long time for me.
    Very disapointed this time.

    5
    这对你有多重要?
  10. cancel or change the order while it is in processing status

    Can you offer the possibility to cancel or change an order while it is in processing status please ?

    5
    0 条评论  ·  I wish  ·  管理员 →
    这对你有多重要?
  11. Live chat

    Live chat. Response rate to messages sent is very slow

    5
    这对你有多重要?
  12. Support ODB++ file format

    It would be very nice if you could handle ODB++ format also.
    From my point of view, it is very easy to work with. After "I saw the light" with this format (compared to gerber), I prefer not to use gerber.

    5
    这对你有多重要?
  13. Customer dissatisfaction

    I can not reply to posts. I will tell my forum this subject countries. http://www.picproje.org

    I said you're a reliable company. Because you do not take into account the customer. You do not give value. Five days I'm struggling on you.

    5
    0 条评论  ·  I wish  ·  管理员 →
    这对你有多重要?
  14. Sensor board, or arduino shield, based on the AS3935 chip

    The AS3935 has a very sensitive lightning detector with SPI and I2C interfaces and needs only a few other parts. Putting this chip on a sensor or shield would make it very easy to build an Arduino lightning detector that could count lightning strikes, log them, and warn of a coming lightning storm. Would be great for a weather station project too.

    5
    这对你有多重要?
  15. Addition of biometric scanner

    Add Secugen Hamster Plus fingerprint scanner to your inventory

    4
    这对你有多重要?
  16. Make the DMX512 PCB board finish flush with the edge of the three pin socket

    When trying to mount the DMX512 board I had to cut off 3mm of PCB to allow the socket to sit flush with the mounting hole.

    Please finish the PCB flush and put a mount hole on the side instead. Note, I'd put it on the side of the high screw hole to stop socket twisting on insertion of lead. Photos attached

    4
    这对你有多重要?
  17. Your online BOM List can not be filled. Please fix it.

    Bom list can not be filled online. Online list does't show.

    4
    1 条评论  ·  I wish  ·  管理员 →
    这对你有多重要?
  18. 4
    这对你有多重要?
  19. BB green in a USB stick compact version - cost reduction could allow volume use for end user consumer products

    BB green in a USB stick compact version - cost reduction could allow volume use for end user consumer products. What could be the cost in 10,000 volume?

    4
    这对你有多重要?
  20. drill dia.

    upto 7.5mm drill diameter in fusion pcb

    4
    这对你有多重要?
  • 看不到你的想法?

My Seeed Idea

分类

反馈和知识库