My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
554 找到的结果
-
Email to Track and Trace number as soons as it comes available
Why I get an email to my order is traceable, but first I have to log in and go to the order history and there find the number.
Why not send the track and trace number in the email?4 票 -
Add Mesh Support to Smart 7688 Duo
The ability to be both a Wifi station and a Wifi access point, simultaneously, would allow the Smart 7688 Duo to participate in powerful Mesh Networks. This can be accomplished virtually within a single radio (allowing for the same channel, or a more power-draining second radio). The 'hostapd' package in openwrt's Chaos Calmer supports this feature.
4 票 -
include SOME documentation with retail products.
I bought a relay shield at Radio Shack and it came with ZERO documentation. How much would it cost you to include a single small sheet of paper? That is all it would take. Even if you included a link to the docs on the box - that would cost you even less. But NOTHING? That is ridiculous.
4 票 -
Release 3D-files for Wio link, Wio node and compatible grove sensors to make it easier for users to create their own 3D-printable casings
Release 3D-files for Wio link, Wio node and compatible grove sensors to make it easier for users to create their own 3D-printable casings and holders.
4 票 -
4 票
-
Need to know if there is free shipping to Beijing
I urgently need to know if there is any free shipping to Beijing area.
Also Transit time and if there is no free shipping then cost to shipping Beijing.
4 票 -
Beagle Bone Green Wireless Without the Dual Stacked USB Connectors
The Beagle Bone Green Wireless is a great idea for several reasons. One thing I was looking for was to get ride of the bulky Ethernet connector. This is an embedded board that is already big, because of the .1" headers, it is humongous in height because of the Ethernet connector.
And so when the wireless version came out I was ex-tactic for a second until I realised you added 2 dual stacked USB connectors?!?!
Please leave the choice to the user to decide whether or not they need that much real estate wasted.People who have enough space for…
4 票 -
Orange Color PCB
I'd like the color orange added for the solder mask.
Thanks
4 票 -
Extension Cable for Grove
I wish there was a male-female Grove cable with, let's say, 100 cm as a extesion cable. Alternatively a tiny male-male PCB could act as an "extension adapter".
4 票 -
Persistence of Vision Board.
Peristence of Vision Board.
Hi I'd like to share a project of Persitence of Vision: Arduino code generator for images and text. It is DIY cheap and easy, and all resources are free.(load any image and it gearates the code)
http://persistenceofvisionproject.com/
Thanks.
4 票 -
Are you planning to sell something using nrf52840 (raytac MDBT50_module for example)?
To use some module with nrf52840
4 票 -
DHL Parcel Germany for International don`t let me a notification for the next delivery day
you need a control for
DHL Parcel Germany for International they don`t let a notification for the next delivery day.
i. e a proof to make a call to the costumer4 票 -
I am still waiting
2018-01-13 04:40:00Arrived at Delivery Facility in FRANKFURT - GERMANY
2018-01-12 04:29:00[FRANKFURT - GERMANY]Shipment on hold
2018-01-11 04:33:00[FRANKFURT - GERMANY]Shipment on hold
2018-01-10 04:35:00[FRANKFURT - GERMANY]Shipment on hold
2018-01-09 04:28:00[FRANKFURT - GERMANY]Shipment on hold
2018-01-08 10:29:00[FRANKFURT - GERMANY]Delivery attempted; recipient not home4 票 -
How to learn ?
404 not found for the music shield v2 wiki page. How to learn?
4 票 -
You are a terrible teacher. A first time customer has no idea how to start. Why do you make it so hard?
Your fist page should show EXACTLY what we need to make things go. So far, I still don't know how this works. The manual for my Grove device says I ned a Seeeduino board with driver board, but you don't sell those?
4 票 -
Virtual DJ 8
Virtual DJ 8 Free Download With Latest Version. Virtual DJ 8 is most used Dj software in the world.
https://softmega.org/virtual-dj-8/4 票 -
Budget Shipping option
I ordered a few boards a month or so ago and the only shipping options were DHL and I forget what other service but it was even more expensive. Might I suggest a budget shipping option for those customers who are less concerned with longer lead times such as say post. The two board orders I placed cost $13.50 CAD and shipping was $35. Then on top of that the boarder stung me with $26 in tax a duty which I do not understand how they can charge more than the product is worth, a problem I have only ever…
4 票 -
sort OPL items
OPL items should be sorted by some meaningful criteria; it is hard to choose a specific item among 15000 different ones. If it is not possible, it should be possible to download all the data base, let's say in Excell format, an do ourselves the sorting by different criteria (case size, manufacturer, name, etc.)
4 票 -
Wire harnesses assembly
Please add a assembly service for custom wire harnesses
4 票 -
Develop a "gender bender" connector, which allows connection of a 1.2 Meg(5 1/4") floppy drive to a 1.44meg 3 1/2" drive support board.
1.2M floppy drives have an IDE 34 pin edge connector(female).
Usb floppy drive controllers have a 34 pin Female ide connector. Need an adapter: male to Male 34pin (cross connected), or similar to get a 1.2m (5.25") floppy to connect to a 3.5" floppy USB kit.Many users have OLD 1.2m floppies with data, which could be recovered, with a standalone usb reader. in General, READING is all that is needed.
Passive Should cost Maybe $10 retail.4 票
- 看不到你的想法?