My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
554 results found
-
I don't see how it's possible for seeed not to see its email pictures don't download. Surely there must be some way of telling them.
I don't see how it's possible for seeed not to see its email pictures don't download. Surely there must be some way of telling them.
1 vote -
Static URL for teachers' custom Grove starter kit
Offer pre-customized Grove Starter packs for teachers that the teacher can customize so they can give the same URL to each student so they buy exactly what they need for their class.
1 vote -
Fix broken EMG sensor example code!
Fix your broken EMG sensor example code. It will not compile!
1 vote -
MCPCB Service request
You add a Metal Core (MCPCB) option to your already excellent Fusion service.
1 vote -
In order for the netduino to stay alive perhaps build a watchdog shield.
In order for the netduino to stay alive perhaps build a watchdog shield that receives a pulse from netduino via output pin and if the pulse is not received for say 5 minutes the watchdog will awake and send the netduino a pulse that are connected to the reset pin that will reset the device.
1 vote -
test leads with sharp tip
test leads with sharp tip, I suggest a better test tip for the measuring leads, made of a spring loaded test pin as the tip and a plastic pencil body; thus it stays firmly on even very thin pins even when the user looks to the measuring values or screen and the keeping force is not constant
1 vote -
How about data on the Edsion Xadow product such as why things are not working? Also a test to tell you the thing is working? Flashing light.
Flasing lights don't anwer the question if the system is working? The OLED pretty much should have some indication there is power ? Nothing!! My only guess is the thing is bad from out of the box.
1 vote -
I would like to see more Grove Kits/Sensors offerings not associated with a platform. Or maybe a fill your own sensor "bag" of sensors!
I would like to see more Grove Kits/Sensors offerings not associated with a platform. Or maybe a fill your own sensor "bag" of sensors!
1 vote -
Please Stock Netduino Wifi 3
Please Stock Netduino Wifi 3
1 vote -
On the SARK-110 I would like to be able to offset the vertical axis and display the j reactive component rather than the Z impedance.
I have the SARK-110 and need to display the j component with vertical axis zero in the middle of the display. Thank you
1 vote -
Support TI C2000 for Crazyflie
You could allow C2000 launchpad plug into actuators and sensors to control Crazyflie
1 vote -
Grove Lib for Linkit assist 2502 SDK (which also works with Linkit one)
create a grove lib that hooks into the linkit assist 2502 sdk. This lib would work with linkit one as well which would enable more advanced development with the linkit one
1 vote -
3G version of LoNet 808 - Mini GSM/GPRS + GPS Breakout, SKU: 113990107
Simcom based. SIM5320E or another 3G & GPS Simcom chip.
1 vote -
due to this limitation "Minimum inner trace width(for 4 layers) 0.204 8" I can't use QFP with 0.5mm like STM32f407VET6
use same DRU fort 2 layer and 4 layer ? At least for TOP and Botton layer in order to use standart packages.
1 vote -
Make available source code for the Skeleton Bot
- 4WD Hercules Mobile Robotic Platform. Would be very handy currently all wheels travel the same direction? Please upload the code you used to create the car in the video. I dont understand how to control the wheels.
1 vote -
I would to see a GPS Bee with a backup battery. So far every start is a cold start.
I would love to see a GPS Bee with a backup battery. So far every start is a cold start.
1 vote -
Price for printing 10x15cm size Fusion PCBs
Reduce the price of printing 15x10cm size fusion PCBs
1 vote -
Fusion/Seed higher prices now? Why? China's economy is in slump!
Why Fusion/Seeed Studio is squeezing more money of the customers? Prices are higher, while China's economy has crashed!!!!!!
1 vote -
RGB laser diode
Create an RGB laser out of Laser Diodes
1 vote -
easy way to personnalize rephone paper craft box
Send me your box shape for rephone as i could include it into my site http://www.visualkit.com (or in a separate one), and provide an easy way to personnalize it. Or perhaps you prefere do your own ...
1 vote
- Don't see your idea?