My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
147 results found
-
I want to pay extra for options
Dear, I want to pay USD 10 for my PCB project extra because of panel. How can I do this?
1 vote -
A new DSO Quad
New hardware ! 4 real analog channels, 10-12 bit samples, at least 100MS/sec (per channel !). Improved "front end" and significantly more waveform memory (micro SD). Try to maintain the price point.
1 vote -
Your online BOM List can not be filled. Please fix it.
Bom list can not be filled online. Online list does't show.
4 votes -
WS2812B breakout board does not say how many are in the package
http://www.seeedstudio.com/depot/WS2812B-LED-Breakout-Board-p-2010.html
I can't figure out how many I'm going to get, because it doesn't say. The picture shows five, but one commenter received only one. Please add a number to the description saying how many WS2812B breakout boards I will receive if I order one unit.
2 votes -
3 votes
-
USB or Grove barcode readers
Need some USB or Grove barcode readers that can be used with BeagleBoneGreen.
3 votes -
e-ink or oled starter kit
arduino to make mimi bt display unit and connect to mobile
1 vote -
Free talk at FSOSS "fRephone" http://fsoss.senecac.on.ca/2015/schedule
I could talk about Rephone at Seneca in Toronto next week. Ask dumb questions and become undumbina-ted
1 vote -
1 vote
-
More Cameras
More inexpensive-yet-good camera modules composed of OVM cameras with flex cables.
1 vote -
easy way to personnalize rephone paper craft box
Send me your box shape for rephone as i could include it into my site http://www.visualkit.com (or in a separate one), and provide an easy way to personnalize it. Or perhaps you prefere do your own ...
1 vote -
RGB laser diode
Create an RGB laser out of Laser Diodes
1 vote -
Price for printing 10x15cm size Fusion PCBs
Reduce the price of printing 15x10cm size fusion PCBs
1 vote -
due to this limitation "Minimum inner trace width(for 4 layers) 0.204 8" I can't use QFP with 0.5mm like STM32f407VET6
use same DRU fort 2 layer and 4 layer ? At least for TOP and Botton layer in order to use standart packages.
1 vote -
Wireless charging for Super Capacitor
A wireless charger that can charge a Super Capacitor [SC]. It would have an adjustable maximum voltage of 2.0 to 2.5 volts, and be able to dump large amounts of current [5A or more -- much more] into an extremely low impedance load [i.e. a current source with an upper voltage limit]. Also, it should be able to dump current into the SC at full bore all the way up to the maximum voltage. A typical SC has a maximum voltage of 2.7 volts, but should not be charged higher than around 2.2 to 2.5 volts [the higher the voltage…
3 votes -
test leads with sharp tip
test leads with sharp tip, I suggest a better test tip for the measuring leads, made of a spring loaded test pin as the tip and a plastic pencil body; thus it stays firmly on even very thin pins even when the user looks to the measuring values or screen and the keeping force is not constant
1 vote -
Shipping needs major work
I had known it would take almost a week to send my order i would have ordered elsewhere.
6 votes -
gerber viewer checked drills
Check drills file in gerber viewer
2 votes -
I wish an I/O expander with i2c
I wish an I/O expander with i2c such as the NXP PCA9502 as an Xadow Modul. the Xadow requires a possibility of additional I / O pins. This can make the Xadow more popular because he would be more flexible. the i2c address may be set via solder joints on the back.
greeting,
avoid1 vote -
Customer dissatisfaction
I can not reply to posts. I will tell my forum this subject countries. http://www.picproje.org
I said you're a reliable company. Because you do not take into account the customer. You do not give value. Five days I'm struggling on you.
5 votes
- Don't see your idea?