My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
Test Your Webpage
For years everything worked seamlessly but now the webpage is full of bugs. Next to the user icon it shows "Hi,?????". Trying to order a Fusion PCB with Firefox everything works, except the "Add to Cart" button does nothing, I tried with 2 versions of FF. With Chromium the menu doesn't work, nothing happens if I move the mouse pointer to the "Fusion" menu. Pressing the mouse button opens the menu, but releasing it goes to a different page. Some links give a 504 error. My address book is empty and all old orders are gone too.
Please install a…3 votes -
Liquid density and temperature sensor (sterilizable)
An addressable, 1 or 2-wire protocol reporting sensor that, when placed in a liquid could report on the temperature and density of that liquid.
This sensor could be used to determine specific gravity during brewing etc.
Also, as a secondary wish - adding a pH sensor would be awesome.
3 votes -
Can you make the LinkIt 7688 with more flash memory? There is not a lot of space for software. Less RAM would not be a problem.
Can you make the LinkIt 7688 with more flash memory? There is not a lot of space for software. Less RAM would not be a problem
1 vote -
new connectors needed
flat cable 2x40 pins low cost IDE specs
connector male IDE 2x40 specs, to construct flat cable connection
to mate with Mega edge connector
connector 2x8 female IDE connector for flat cablesmale connectors and male pins to construct Grove connector
RC plane (yes airplane) LI-PO battery connectors male females with male/females pins to construct longer cable connection
ONE to Many connector like 2- input female pins to insert to connector with connector other side has 8 output to insert male or female pins, called distribution connector, just like the black 0.1"(2.54mm) crimp connector.
this connector does not exists yet…1 vote -
Beaglebone Industrial
It would be nice to have an option where Industrial range components are used on the beaglebone green.
Quickly looking at the BOM, there are four components, all have -40 to +85C equivalents so a relatively simple change.2 votes -
"Processing" is not a very descriptive way of telling me where my project is at.
I can't see any deeper information than that my project is "processing" what does this mean? When can I expect it to change?
1 vote -
No pagination would be great, instead use "infinite" scroll
I really don't like browsing in paginated overview pages
3 votes -
add re order tap to PCB order history (ie as it was).
add re order tap to PCB order history (ie as it was).
2 votes -
Create some nordic semiconductor nrf52 board.
Some small beacon-like nrf52 board. Like armstart one for nrf51
1 vote -
Electrical Conductivity Sensor
It seems to me like the only thing you guys are missing for building a hydroponics environment monitor with Grove is the Electrical Conductivity sensor. I'm working on building such a monitor and it'd be great to use Grove for it :)
1 vote -
Adapt your code for RGB matrix ?
Hi,
I need a pilot board for a 64x32 RGB Leb Matrix. I saw your matrix driver board here : http://www.seeedstudio.com/item_detail.html?p_id=2645
But it doesn't seem to pilot RGB matrix... only RED and GREEN matrix. Is it possible to adapt the code for this ?
Thanks,
Mike
1 vote -
Tech Support Page Not Working
I noticed that when I enter information on the tech support page that I get error 405 - Not allowed.
Can you please fix that problem?
1 vote -
new customer
set terms with seedstudio to make purchases
1 vote -
Correct your weeb page
http://www.seeedstudio.com/service/index.php?r=pcb&ref=banner_fusion_fusion201631
in this page it says 4.9$ for 10 pcs but when you click it it changes to $9.9
why it is different ?3 votes -
Adapter Boards
I would like to be able to put smaller pitch components onto a regular breadboard.
Currently I have a number of leads from a mother board that fit very small pitch connectors. I need to be able to breakout these headers to fit onto a regular breadboard.
I cannot even find prototype boards with other than 2.54 pitch holes, let alone a dual size board.
Adapter boards that allow a dual row small pitch header to be fitted that breakout to standard size would be great. Currently I have 16 pin, 8 pin and 6 pin dual row headers that…1 vote -
Data storage expansion for the RePhone.
It would be great to be able to expand the RePhone memory, either to have a module that increases the flash memory or a module for a SD card reader, anything that could increase the only 5mb storage that is available in the RePhone.
3 votes -
Accumulate Order
Your recent Flash Sales are great, but if I could pay for then combine my orders from multiple flash sales then I can save on postage costs and pay postage separately at the end. But it does mean you will need to set aside each order until the end or give buyer option.
1 vote -
Make an HC11/12 development kit available.
433MHz comms are used by many devices and the 433MHz chip on the HC12 has a lot of capabilities. If an IDE were available then the HC12 board could be adapted by developers for purposes beyond the standard FU1/2/3 usage.
2 votes -
Linkit Assist 2502 Wiki and Projects
Complete support and Wiki page for Linkit Assist 2502. It says it works with xadow but nothing is clear in the manual provided by mediatek and not even a single project image or video on the internet. Makes me skeptical whether to buy the kit or not because after buying it, I won't be able to know how to handle it.
1 vote -
Official Raspberry Pi Touchscreen - Power bridge
Official touchscreen has a long jumper cable for power.
This can be much nicer with two small PCBs.
There may also be a micro-usb connector for the power supply.1 vote
- Don't see your idea?