I wish an I/O expander with i2c
I wish an I/O expander with i2c such as the NXP PCA9502 as an Xadow Modul. the Xadow requires a possibility of additional I / O pins. This can make the Xadow more popular because he would be more flexible. the i2c address may be set via solder joints on the back.
greeting,
avoid
1
vote
![](http://www.gravatar.com/avatar/ea077cef0caaeb97efdef3724e09163b?size=40&default=https%3A%2F%2Fassets.uvcdn.com%2Fpkg%2Fadmin%2Ficons%2Fuser_70-6bcf9e08938533adb9bac95c3e487cb2a6d4a32f890ca6fdc82e3072e0ea0368.png)
-
Barry Flash commented
I have it with a code example and a picture posted in the forum.
https://freemoviesite.me/ -
avoid commented
I have made with the PCF8574AP and Xadow breakout a try. it works well.
I have it with a code example and a picture posted in the forum.
http://www.seeedstudio.com/forum/viewtopic.php?f=43&t=5970