Mbed web compiler support for nrf51 Seeed Mirco BLE SoC
Please add the nrf51822 Seeed Micro BLE to the mbed web compiler. I see the Seeed Arch BLE in the web compiler, they have a similar/same pin map. Also since the Micro BLE has no USB upload firmward, to make this easy, allow update via FOTA.
mbed already has an nrf51288 device in the web compiler with FOTA, so you need to take this and use the arch/micro ble pin mappings.
http://developer.mbed.org/platforms/Nordic-nRF51822-FOTA/
"xiongyihui" should be the guy to talk to
Thanks,
Shane
3
votes
drksun
shared this idea