My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
554 找到的结果
-
New Seeed Fusion Interface
Your new user interface for ordering is VERY bad and not well thought out. Submitting an order gets you to a page which says to close the window with no close button.
Payment screens are not clear and displayed shipping address has garbage characters. I don't think you have initialized the data fields.
Cost numbers do not have two decimal digits for North American display. Check your usage of UNICODE is not correct.
Go back to the previous interface and fix these problems, test, then release.
1 票 -
Re-order
Re-order from old bazaar history
1 票 -
WebSite Bug Report: Cart Icon not updating
I had three PCBs loaded in the cart, yet the little icon (upper right corner) still showed '1', then added 4th PCB and shopping cart icon finally incremented to '3' -- but still not correct!
1 票 -
new connectors needed
flat cable 2x40 pins low cost IDE specs
connector male IDE 2x40 specs, to construct flat cable connection
to mate with Mega edge connector
connector 2x8 female IDE connector for flat cablesmale connectors and male pins to construct Grove connector
RC plane (yes airplane) LI-PO battery connectors male females with male/females pins to construct longer cable connection
ONE to Many connector like 2- input female pins to insert to connector with connector other side has 8 output to insert male or female pins, called distribution connector, just like the black 0.1"(2.54mm) crimp connector.
this connector does not exists yet…1 票 -
Fix you emails so that the pictures work. Fix customer support so that the verification works!!!
Fix you emails so that the pictures work in Firefox browser. Fix customer support so that it works when you put in the correct verification code (absolutely sure that I did) !!!
1 票 -
It would be very very good if PCB calculator would have options for 6/8 layer PCBs.
It is available on competitor sites and it is bad that it is not available here
1 票 -
Fix the shipping information page.
The language of the shipping information page is unclear. Is shipping free or only free if over $200? Does free shipping apply to Fusion PCB service? If not, what are the costs?
1 票 -
pdf link is fail
https://www.seeedstudio.com/SIM808-GSM%26GPRS-%2B-GPS-Module-p-2523.html
All datasheet link is all failure.
1 票 -
to correct the shipping date
i could be usefull to correct the shipping date in order to track the product.
Thanks :)
1 票 -
ESP8266 + SDcard + Arduino bootloader = 10$ arduino-compatible standalone datalogger
The ESP8266 can be re-flashed to allow uploading Arduino skecthes.
It also has native support for SD card.
So, a single board which includes ESP8266, an SDcard reader and battery connector would be a cool, wifi and cheap standalone datalogger (no need for external MCU).
ESP3212, just arrived to the market, even supports Bluetooth!1 票 -
Special programming board for ESP-xx modules
All current ESP8266-based boards lack an important feature: the ability to remove the ESP (ESP-01 to ESP-12) module from the programmer board after programming the module.
A board with specific solderless socket for ESP modules would be very useful.But please don't forget to make the board not larger than 23mm or it will not fit into breadboards, like many "fake" boards available now.
1 票 -
Mobile site displays incorrectly
On my moto G3, the mobile site displays incorrectly. There is a big white box over the majority of the text, and the font is too small for this screen.
I sometimes wonder why bother making a mobile site when it's just rubbish?
1 票 -
Your articles don't make english
The English in some of your articles doesn't make sense (e.g. http://seeed.cc/Are-these-issues-often-overlooked-in-the-development-of-hardware%3F-t-6200.html). Perhaps ask any native English speaker to make it readable.
1 票 -
DSO Touch Users Guide in Japanese
I translated the manual into Japanese.
See
http://wp.me/p67nSb-3vvThanx,
1 票 -
Have you considered making a Grove Interface board for the Micromite computers? These are made in Australia and being cloned in US & UK
There is a new version of the Micromite called the Explore 100 as well as a new one called the Micromite Plus LCD Backpack both of which would be amendable to a Grove interface. The Explore 100 has two MikroElectronika Interfaces which is not enough and they are too expensive compared to Grove. A grove interface would be fantastic.
1 票 -
Make A Grove Oscillator Board based on Si5351 using I2C interface
This board could form the basis of VFO or Antenna Analyser ccts and possibly numerous other ccts requiring a computer controlled oscillators such as SDR Radios etc
1 票 -
not notify the customer that PCB has been shipped unless it has actually been handed over to the courier such as Fedex.
I got email from you saying my PCB has been shipped in Nov. 2. But Fedex record shows it only received it on Nov. 8, and they delivered it to me the next day, Nov 9. So there is unexplained delay of almost a week. Better to notify me the day you actually handed the PCB over to Fedex as ship date.
1 票 -
It would be great if your ads used proper english, ie: life not live
It would be great if your ads used proper english, ie: life not live
1 票 -
161206023299
dont do anything
1 票 -
Would love to see dust detecting sensors/thin/tiny/slim/sleekish with IoT features.
Would love to see dust detecting sensors/thin/tiny/slim/sleekish with IoT features. You may ping me if anyone have done any prototyping, POC etc. to me at niha at akkob
1 票
- 看不到你的想法?