I suggest Seeed...

BitCoin payment option would be great!

106 votes
Vote
Sign in
Check!
(thinking…)
Reset
or sign in with
  • facebook
  • google
    Password icon
    Signed in as (Sign out)
    You have left! (?) (thinking…)
    Anonymous shared this idea  ·   ·  Admin →

    11 comments

    Sign in
    Check!
    (thinking…)
    Reset
    or sign in with
    • facebook
    • google
      Password icon
      Signed in as (Sign out)
      Submitting...
      • Anonymous commented  · 

        I will go a step further and it is considering no only in acepting ether and bitcoin as an altenative payment but also acept participate in ICO as a Beneficiary (Independent (pre-paid) Dynamic Beneficiaries

        https://media.consensys.net/exploring-continuous-token-models-towards-a-million-networks-of-value-fff153175776

        We are developing an ICO where the investor finances the IoT device (made by seeed Studio) and in exchange gets a % of the revenue that the IoT device produces under smart contract in its life cycle so in order to built credibility into the ICO token the ether will be released directly to the IoT manufacturer under Smart Contract once the first batch is registered into the Ethereum blockchain as a Proof of Existence

      • Anonymous commented  · 

        There are a number of third-party services which handle Bitcoin payment processing into regular currencies, that might make implementing this easier and safer for you.

        While many people won't use it, I don't really see any valid reason NOT to add it, and accepting it while other sites don't gives you an advantage attracting customers.

      • Bob commented  · 

        If paypal is complicated for you, then you must be a fifth-grader.
        Forget bitcoin, its for money laundering only.

      • Chris S. commented  · 

        Please add Bitcoin. I'd use it regularly just like I do with Fasttech.com. I often get paid in BTC so being able to spend it without dealing with paypal (which is complicated for me) would be awesome. You can integrate it using Bitpay as many do (including Fasttech).

      • Anonymous commented  · 

        I would definetely buy in bitcoins if this site supports it.

      • Simon Peacock commented  · 

        Forget Bitcoin. Although bitcoin is a cool idea, without government acceptance it lends itself to money laundering and criminal activity, transactions will eventually be blocked (somehow) or bitcoins will be traced back to a criminal event in which case the bitcoin would be treated as stolen property and forfeited.

      • Gitle M commented  · 

        Bitcoin support would be great. If you as the first low cost PCBA supplier accept bitcoin, you would gain me as a loyal customer.

        The commenter below me is missing the point, Paypal may work well for him, but it doesn't for everybody, that's just a fact. There are several countries where paypal is simply unavailable, and yet others may choose to avoid it for various reasons. By accepting bitcoin you would increase the amount of potential customers, and its core userbase perfectly aligns with your target audience: engineers and other tech savvy people.

      • Graham commented  · 

        Forget bitcoin. There's nothing wrong with PayPal; I've used it since 2002 with zero problems, as have millions of other people. Anyone who has an issue with PayPal is probably trying to cheat the seller. All of PayPal's problems are connected with suspicious use of funds, admittedly not all of them justified, but buying printed circuits boards is hard to classify as suspicious.

      • Oliver commented  · 

        It would be wiser to find a payment service that automatic converts not only bitcoin but another altcoins as well. More payment options = more costumers. ;)

      • Anonymous commented  · 

        Hi, bitcoin as payment method really would be great since it's the only reasonable method for us in order to buy at seeed bazar or fusion. Paypal is a no-go since it has such a rotten stance. Alipay isn't an option at all for us living in europe. So, please introduce bitcoin.

      Feedback and Knowledge Base