My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
308 找到的结果
-
Which Batteries for which product
Please specify which batteries work with RePhone and WIO - in your store, please
1 票 -
Better inventory management needed
Most products that I would to order are out of stock! :( Water pump, relay, flow sensor, etc. There should be an option for back-order or notification to customer when the product is back in stock.
8 票 -
Fusion PCB Specification -- Provide separation dimensions between layers.
For computing strip-line impedance it is important to know the distance between conducting layers and the dielectric constant of the insulator material. If averages are provided please also provide variance
21 票 -
talk to phone to enter nos only
e-ink display is what we need for sunlight readability
1 票 -
A lot of products with Seeedday coupon are not in stock or discontinued. Very annoying!
A lot of products with Seeedday coupon are not in stock or discontinued. Very annoying!
7 票 -
payment method
Better, more reliable payment method.
3 票 -
Mentor Gerber Format
Complete procedure to get the PCB, Mentor Graphics is the software
1 票 -
provide Documentation in English for ESP8266 module small and a tutorial on web site.
provide Documentation in English for ESP8266 module small and a tutorial on web site. If you sell it in USA you need to provide English documentation.
2 票 -
Impedance Calculation Utility
A calculation tool to let customers know the impedance of their PCB traces.
Here is an example:
http://www.hughescircuits.com/index.php/en/support/impedance-calculatorThe customer would only need to enter their PCB trace width, because all the other parameters can be determined automatically from the PCB specifications that the customer has selected.
10 票 -
Fraud?
I suggest you fix your ordering system!
1) I ordered and paid $398,20 USD.
2) You prepared to ship something for $110.58, so I complained that something is missing.
3) You cancelled my order claiming I did not pay (so your accountant says) and suggested to re-order
4) I sent you my paypal transaction of $398,20 USD and your invoice of 110.58 EUR.
5) and I am waiting for a replyObviously I am not willing to reorder and pay twice.
Regards,
Robert
--
Robert Berger
Embedded Software SpecialistReliable Embedded Systems
Consulting Training Engineering
URL: http://www.reliableembeddedsystems.comsubscribe to Linux…
1 票 -
Add a DTR Pin to the dual mode Bluetooth Device so that it can also flash the microcontroller over the air.
Currently the Bluetooth Modules with HM-13 are not providing the DTR Pin that is needed to reset the microcontroller while flashing a new firmware. It would be great if that functionality could be made available on one of the programmable Output Pins.
1 票 -
Make available source code for the Skeleton Bot
- 4WD Hercules Mobile Robotic Platform. Would be very handy currently all wheels travel the same direction? Please upload the code you used to create the car in the video. I dont understand how to control the wheels.
1 票 -
Fix the translation for the new Mini Soldering Iron
Great product, but the translation needs some work. Here is my suggestion:
Our Mini Soldering Iron, is a small, lightweight, quick heating soldering pencil that is great for many soldering application. The stable temperature is controlled accurately by the embedded STM32 controller and is easily adjusted from 100 to 400 degrees Celsius. You will benefit from dual temperatures, accelerated sensors, included sleep mode, and automatic over-heating warning. Soldering iron tips can be replaced with 4 different types and the embedded software can be reprogramed.
Features:
Portable and lightweight for convenient soldering
Easy temperature control
Sleep mode for safety and extend…2 票 -
I'm having communication problems
Very hard to do business with you. I'm having communication problems. I can not find contacts for communication. I do not have time. I can not spend time with you. I am in a hurry.
I canceled my order and cancel the payment.
8 票 -
Create more longer cables for grove.
Create more longer cables for grove. For example 2 or 5 meters would be really useful. Thanks
9 票 -
Panelize Instruction Improvement
Improve the panelize instructions for Fusion PCB. Currently is very, very, very poor.
5 票 -
stop overcharging for shipping Fusion PCBs
Please charge customers for the correct shipping weight instead of the maximum for PCBs of any given size. Most companies do this.
For an example, Arduino (shield)-sized boards are only one third the size of the 10cm x 10cm board category that must be used to buy them, but they are only ONE THIRD of the size and weight. We have to pay (express) shipping for TRIPLE the weight of the actual order and this can be substantially more expensive.
Please use the actual board size to compute the proper weight. Many other lower-cost PCB prototyping services do this, and…
23 票 -
Bicycle tracking and theft protection
We need a GPS device with GPRS and battery with motion charging small enough to fit inside a bicycle seat post. Or maybe fit underneath bicycle seat. When in motion it must charge the battery and transmit GPS coordinates every 30 sec via GPRS(sim card installed)
2 票 -
LoNet - GSM/GPRS/GPS Breakout
More documentation
9 票 -
Arduino Dial Up Modem shield
Dial Up modem's days are long gone but Land line still exists either in the form of home pbx or PSTN, An Arduino based Dial Up modem shield can be used for a lot of fun projects.
Modem chips are already available with AT Command support
Currently there is no shield to interface arduino with phone line
This shield can also become a base for Arduino corded telephony with additional sheilds for setting up arduino based Home PABX e.g 4 port intercom shield or Voip shield12 票That’s a gooood idea, we’re going to start it from forum.
- 看不到你的想法?