My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
308 找到的结果
-
Single board computer with embedded 3g modem
I just saw the RePhone and the Linkit One, but these are powered by microcontrollers, why not develop a single board computer like the Beaglebone green or Raspberry Pi but with an embedded 3G modem and LiPo battery support
2 票 -
HS code
you should post an option of "the number of harmonized system code or the number of tarif code" for international purchases.
3 票 -
Give price breaks for large quantity purchase
I don't see any price breaks for large quantity orders.
10 票 -
Fix you Stalker V3 Defect
fix your P5 defect on the Stalker V3
1 票 -
Seeeduino 1284P
I would like a Seeeduino 1284P. I really like Seeed's configuration of
the mega better than arduino's, however I feel that the 1284p has
the right amount of I/O and storage with more RAM than the 2560.3 票 -
A decent customer service.
A decent customer service.
2 票 -
Grove Lib for Linkit assist 2502 SDK (which also works with Linkit one)
create a grove lib that hooks into the linkit assist 2502 sdk. This lib would work with linkit one as well which would enable more advanced development with the linkit one
1 票 -
Support TI C2000 for Crazyflie
You could allow C2000 launchpad plug into actuators and sensors to control Crazyflie
1 票 -
On the SARK-110 I would like to be able to offset the vertical axis and display the j reactive component rather than the Z impedance.
I have the SARK-110 and need to display the j component with vertical axis zero in the middle of the display. Thank you
1 票 -
Gerber Viewer doesn't show holes.
Worried that Seeed may not see the drill files in my Gerber.
6 票 -
Fusion PCB pricing
PCB should be priced by the total sq cm used & not by fixed length & width measurements. This would stop crazy price jumps. Build a board that is 5.54cm & you have to move up to 10cm size board pricing. This crazy & shouldn't be happening. Please price your boards fairer for the total area of the boards used & not for the area not used.
29 票 -
I would like to see more Grove Kits/Sensors offerings not associated with a platform. Or maybe a fill your own sensor "bag" of sensors!
I would like to see more Grove Kits/Sensors offerings not associated with a platform. Or maybe a fill your own sensor "bag" of sensors!
1 票 -
MCPCB Service request
You add a Metal Core (MCPCB) option to your already excellent Fusion service.
1 票 -
Fix broken EMG sensor example code!
Fix your broken EMG sensor example code. It will not compile!
1 票 -
Order Number: 154481
The problem is still not resolved. Waiting for your attention.
Your customer service is progressing very slowly. Problem solving long.
13 票 -
Addition of biometric scanner
Add Secugen Hamster Plus fingerprint scanner to your inventory
4 票 -
Static URL for teachers' custom Grove starter kit
Offer pre-customized Grove Starter packs for teachers that the teacher can customize so they can give the same URL to each student so they buy exactly what they need for their class.
1 票 -
I don't see how it's possible for seeed not to see its email pictures don't download. Surely there must be some way of telling them.
I don't see how it's possible for seeed not to see its email pictures don't download. Surely there must be some way of telling them.
1 票 -
Fix the recipe interface
I have a lot of trouble getting through the recipe process.
It is extremely buggy. The ability to post formatted Arduino code to the recipe would also be nice.Maybe put a sign up to say "under construction" on this section before anyone else goes through the same pain that I just went through.
1 票 -
The 'Contact Support' link to the right doesn't work.
I need to change my shipping address and can't contact customer support because the link doesn't work
2 票
- 看不到你的想法?