4WD Mecanum Wheel Robot Kit (SKU: 110070012)

Q1: What battery do you recommend to drive the motors? Do you sell this battery?
A1: We recommend you to use 2200mAh-7.4V Lithium Battery. We do not sell batteries separately.

Q2: Can this vehicle run straight after assembly? Is the Program pre-loaded into the controller?
A2: The moving direction depends on the coding. The kit does not contain the controller.

反馈和知识库