ESP8266 based WiFi module - SPI supported (SKU: 317060015)

Q1: In "ESP-12E Brief Spec", "Pins Table" the "MOSI" pins is 10 and in "Reference Schematic" the "MOSI" pins is 9. Which is the correct pin number?
A1: Correct Pin numbers are as follows.
MOSI: Pin13
MISO: Pin10

反馈和知识库