Xadow GSM + BLE (SKU: 102040005)

Q1: What is the power consumption of Xadow GSM + BLE?
A1: The power consumption depends on the modules connected with it and the frequency of using them. Normally for Re phone kit, the 520mAh battery lasts about 5-6 hours with the display fully working and during standby it would last about 1-2 days. The current is 1.6mA when GSM is shutdown.

反馈和知识库